2010-07-26 2:22 AM
I2C Unable to receive start state (EV5)
#i2c #i2c #i2c-gpio #stm32-i2c-master2011-07-15 4:39 PM
We too are facing the same problem as you do. We are using STM32F103R8 controller.
We tried to do timeouts and then reset the I2C bus, but that does not help it recover. We first thought it was the slave not responding but it took us a lot of time to find that the controller is the culprit. We see that the I2C is stuck up in the while loop waiting for the ack from the slave (EV6) after sending the slave address on the bus.
Could you please tell us if you have found a soultion to this I2C stuck up in EV6 loop issue.
2013-12-09 9:13 AM
Hello,
any solution to this problem. I also get stuck in the while loop. I have two I2C devices on the bus (0x50 and 0x60). I can read and write to one device,and also write to the other, but i cannot read from it. I am using 4k7 pullups with ~3.0 V VDD (the output on VDD when connected to USB supply - using stm32l discovery). Anyone got some information,I would be very grateful. Best regards,KWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.