2013-07-15 12:40 PM
Hello I am working on a project that uses FSMC .Everything is fine when I use 16bit mode but in every write i need to shift the data <<8 to bring it on to the D8-D15 lines . I cant use DMA like this . so i need a way to write the data in 8bits. my LCD is 8 bits.
FSMC_MemoryDataWidth=FSMC_MemoryDataWidth_16b;
changed to
FSMC_MemoryDataWidth=FSMC_MemoryDataWidth_8b; but no sucess.
i have checked the hardware connections it seems all right.
Thanks for any help.
#fsmc-in-8-bit-not-working
2013-07-16 12:33 AM
Connect the LCD to D0-D7.
JW2013-07-16 4:50 AM
thanks for your replay but i have Already done that but that doesn't work .can you please describe the differences that occur in 8 bit and 16 bit mode.
2013-07-17 3:33 AM
I solved it myself
1: declared 8 bit data width.2:removed R41 and R423:voltage levels on PE are little(3.00 while rest 2.90) higher than vdd added some registers to control it.2013-07-17 4:37 AM
> 2:removed R41 and R42
Strange. I did use the STM32F4Discovery with a display through 8-bit FSMC, and did not remove R41 and R42, and experienced no problem with that. How did you set the speed (GPIOx_OSPEEDR) on those pins? JW2013-07-18 10:51 PM
pulling those pins UP makes a problem i,e they stay in high level even if i send zeros.
that's why i pulled those down and removed the registers. GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC); //NWE GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC);// GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_FSMC);// GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_FSMC);// GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_FSMC);// GPIO_PinAFConfig(GPIOD, GPIO_PinSource11, GPIO_AF_FSMC);//required for fsmc line in lcd's DC line GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 |GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_14 |GPIO_Pin_15;//edit this line GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; //added GPIO_Init(GPIOD, &GPIO_InitStructure);2013-11-28 6:19 AM
Hello everyone,
I have a similar problem: I'm trying to add some more SRAM memory to my STM32F4 Discovery board. It is 8Mb SRAM named AS6C8008-55ZIN with 8b data bus width. I connected it to my FSMC interface with multiplexed 8b data bus mode. A0-A7 is avaliable through 8b buffer 74HC573. With this setup i couldn't write and read anything from my memory. I tried several timing's , checking all signals with oscyloscope , but everything was fine - still the memory was unable to show me anything. I decided to change data bus width in fsmc settings to 16b , just to try it out. Guess what , it worked. The problem is : I can't get access to odd addresses starting from 0x60000001. Even addresses are fine , i can write and read anything ( yet i'm still using 8b words) . Is it the problem with R41 and R42? What am I doing wrong? here is my fsmc config: FSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure; FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure; //----------------------------------------- // Clock Enable //----------------------------------------- RCC_AHB3PeriphClockCmd(RCC_AHB3Periph_FSMC, ENABLE); FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 4; FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 11; FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 5; FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 15; FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 0; FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0; FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A; FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1; FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Enable; FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_SRAM; FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b; FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable; FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low; FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable; FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable; FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable; FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE);2013-12-09 7:52 AM
fsmc works quite fast so always make sure to check the timings are OK.make a little delay (10cycles) in between the commands and data .Thats what i did and it solved all the problems .now there is no problem with R41 R42.it all works with them and without them.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.