2014-08-04 10:53 PM
Hi All,
I am having an issue with I2C on the STM32F4. After successfully transmitting an address byte with values below 0xF0 , but when address value is more or equal 0xF0 (e.g. 0xF0, 0xF2, 0xF4 ..) - the slave acknowledging After the first byte of I2C transaction(As it should do) and cause error by the Acknowledge failure flag. Here is the wave from that I capture(As you can see that the transaction hang after first byte):We’re moving the ST Community to a new platform to give you a better and more reliable community experience.