cancel
Showing results for 
Search instead for 
Did you mean: 

Bugreport Cube32MX 4.0 & HAL_UART_TxHalfCpltCallback

Osto
Senior
Posted on August 02, 2014 at 08:21

Hi,

In the HAL documentation, stm32fxx_hal_uart.c & .h, I can read that in interrupt mode, the HAL_UART_TxHalfCpltCallback is called after half of tx is transfered but this is wrong.

The HAL_UART_TxHalfCpltCallback is only called if I use DMA transfers. Either is the documentation wrong or the function is not implemented to end.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 05, 2014 at 13:06

Hi ostovary.m,

Thanks for the feedback. We’ve noted this as a copy/paste mistake within the driver comments. You're right, the HAL_UART_TxHalfCpltCallback is only called in DMA mode.

We’ll pass you feedback along to our STM32CubeF4 team. Keep an eye out for the next update!

With regards.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.