STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC - EOC flag, DMA, overall conversion time

Posted on July 23, 2014 at 11:42Dear all,I have several questions regarding ADCs in STM32 (more specifically, I use STM32F407ZG). Let me explain you how I use them:1) I have 3 ADCs that are triggered by the same timer (TIM4), and that are used in sc...

marko2 by Associate II
  • 2612 Views
  • 1 replies
  • 0 kudos

STM32F4, SPI with DMA: strange behaviour

Posted on August 05, 2014 at 10:31 Hello , I have successfully implemented a quick and dirty communication between the STM32F407 and an external ADC ADS1278 via the SPI, using DMA. Everything seems to work fine until the moment I try to ...

kostadin by Associate II
  • 1577 Views
  • 2 replies
  • 1 kudos

STM32F072 ADC and DMA Help

Posted on August 05, 2014 at 19:36Hello,I'm new to the concept of using DMA with ADC on STM32F072 MCU and I want to read 6 ADC channels (PA0 thru PA5) using DMA.Initially I tried reading the 6 channels just by configuring the ADC as follows:void Adc...

RTC not running in Stop Mode

Posted on August 05, 2014 at 14:58Using an STM32F103, I want to wake from Stop mode by RTC alarm after 5 seconds.I have set EXTI on UART_RX and #17 for RTC.Here is what I know: I can put the MCU into Stop mode (via WFI).I can wake from Stop via UA...

How to use I2C to ignore NACKs? (stm32f401 vs. SCCB)

Posted on August 05, 2014 at 15:12HiI'm trying to interface an OV7670 module using STM32F401 discovery board. First step is to get this SCCB interface going, which seems to be an I2C ripoff, http://www.ovt.com/download_document.php?type=document&DID...

bgeri91 by Associate
  • 1018 Views
  • 0 replies
  • 0 kudos

STM32F401RE SPI Init without CMSIS Functions

Posted on July 22, 2014 at 10:53 Hello, I have a problem with the initialization of the SPI1 from my STM32F It doesn't work and I don't now what I doing wrong or what I forged. When I write something in the data Register ( SPI1->DR), nothing h...

c239955 by Associate
  • 1508 Views
  • 3 replies
  • 0 kudos

Bugreport Cube32MX 4.0 & HAL_UART_TxHalfCpltCallback

Posted on August 02, 2014 at 08:21Hi,In the HAL documentation, stm32fxx_hal_uart.c & .h, I can read that in interrupt mode, the HAL_UART_TxHalfCpltCallback is called after half of tx is transfered but this is wrong.The HAL_UART_TxHalfCpltCallback is...

Osto by Senior
  • 658 Views
  • 1 replies
  • 0 kudos

I2C Address Issue

Posted on August 05, 2014 at 07:53Hi All, I am having an issue with I2C on the STM32F4. After successfully transmitting an address byte with values below 0xF0 , but when address value is more or equal 0xF0  (e.g. 0xF0, 0xF2, 0xF4 ..) - the slave ack...

0690X00000602stQAA.jpg 0690X00000602w6QAA.jpg 0690X00000602wBQAQ.jpg

Help with simple ADC on STM32F4

Posted on July 17, 2013 at 16:46 Hi all, I'm trying to get a simple ADC working on the stm32f4 discoveryboard. At the moment I simply want to obtain an input value(ConvertedValue) as a variable rather than saving to memory inDMA. I'm struggl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.