2019-11-29 6:50 PM
2020-01-07 5:08 PM
The Keil Lite/Eval version can be downloaded and can build/debug 32KB of code
The ST-LINK/V2 would be one of the cheaper and more flexible debug pods.
2020-01-07 5:17 PM
Thanks, will order the ST-LINK/V2 and start
2020-01-20 6:14 PM
Got ST-LINK/V2. Tried to start following instr:1 Launch UVision - OK. 2 OPEN A PROJECT FOR AN STM32 DEVICE, Opened OK but could not find STM Device in the database. So could not start instr 3 - Open the project config Project -Options for target.
2020-01-20 9:17 PM
Keil would presumably need to pull "Packs" to support the STM32G4.
After it says it can't find the devices, go into the Pack Installer by clicking the 3 coloured dice icon
Try building one of the CubeG4 examples.
2020-01-22 5:35 PM
No Luck. Went to pack installer, has a list of devices on the left one of which was mine STM32G474VET6. tRIED TO INSTALL BUT GOT 404 ERROR.
2020-01-22 5:43 PM
I HAVE 2 SCREENS working, one is keil Uvision, the second is pack installer which has a left subscreen with 2 tabs devices, boards and a right subscreen with 2 tabs packs, examples. The left subscreen has a list of devices including 32g474vet6, but if I select this dervice, get 404
2020-01-22 6:01 PM
Could not see the 3 coloured dice icon, may be I am in the wrong screen?
2020-01-25 1:03 PM
Was able to build
STM32Cube_FW_G4_V1.1.0\Projects\STM32G474E-EVAL\Examples\CRC\CRC_Example
and also after changing device to STM32G474VETx
2020-01-26 3:59 PM
THANKS. No help to me as I can't seem to get past the 2nd step in 'using ST-LINK in Keil MDK QUICK START GUIDE" i.e. Step 1 - Launch UVision - OK
2 - OPEN A PROJECT with an stm32 target device - tried this i.e. Open Project but does not give me my target device i.e. STM32G474VET6.
I am not using a dev board but MY OWN board already assembled with the VET6
2020-02-08 2:23 PM
Still struggling!
Surprised there are no clear instructions on how to run this. I d'loaded it and it appears as an icon on my desktop titled MDK529.exe. I click on this icon expecting it to run but instead get a msg - 'this pack is already installed'. So how to run the devicepack is still a mystery. I am not running the eval board but am trying on an STM32G4 installed on my own board. Guess with the STM debugger (STLINK - V2) should be no different
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.