2019-11-29 6:50 PM
2019-12-19 5:34 PM
You really could not find the ST-LINK debuggers? Shame on Google ((
https://www.st.com/en/development-tools/st-link-v2.html
-- pa
2019-12-20 8:46 AM
Thanks. This shows a 14-pin connector; mine has 20-pin, so trying to figure this out.
2019-12-21 9:45 AM
Additional nice option:
https://www.segger.com/products/debug-probes/j-link/models/j-link-edu-mini/
> Thought this was a helpful site.
Helpful doesn't mean other people wasting their time on basic Google searches for you only because you are too lazy to do it and read something.
2019-12-21 10:53 AM
Here are all connectors: 20 pin, 10 pin
http://www.keil.com/support/man/docs/ulinkpro/ulinkpro_cs_connectors.htm
2019-12-21 11:05 AM
"20-pin JTAG header" Should pull up images and details
http://www2.keil.com/coresight/coresight-connectors/
The ST-LINK/V2 pod has a 20-pin header/ribbon cable. Ditto Segger J-Link, and Keil's uLink
JTAG is a standardized method of getting data in/out of a chip for test purposes. It is basically a "Scan-Chain" that provides secondary access to logic FLIP-FLOPs throughout the device, allowing data/states to be shifted in, and later shifted out. Perhaps there is a WikiPedia page on this.
https://en.wikipedia.org/wiki/Scan_chain
https://en.wikipedia.org/wiki/JTAG
ARM uses it as a method to access sections of the CPU core. It is built in to the silicon design, not software. The header provides for a standard means of connectivity. Several vendors have their own implementation, or connectors. The ST-LINK/V3 uses either an ARM 10-pin SWD/JTAG header, or ST's expansion on that, which also provides for UART connectivity.
You need an external pod to provide ready access to this interface. Host side debugger software interfaces via the external pod. These things tend to be external so as not to burden the IC with unnecessary HW/SW for the debug/development use case, ie not needed for the millions/billions of parts in end user products beyond programming at factory.
2019-12-21 11:12 AM
http://www2.keil.com/coresight/coresight-connectors/#20pin
2019-12-21 2:06 PM
Thanks to all who provided helpful replies: As I see it this is all I need:
2019-12-21 2:29 PM
Also: https://en.wikipedia.org/wiki/List_of_ARM_Cortex-M_development_tools
2019-12-21 3:18 PM
https://www.mouser.com/ProductDetail/STMicroelectronics/ST-LINK-V2
Writing code Keil, or whatever the exiting engineers were using. Keil will support ST-LINK, J-LINK or u-LINK debug pod for purposes of programming/debugging
"Programming" the physical device with a .BIN or .HEX file, use ST-LINK Utilities, or STM32 Cube Programmer.
https://www.st.com/en/development-tools/stm32cubeprog.html
https://www.st.com/en/development-tools/stsw-link004.html
2020-01-07 3:59 PM
Thanks. Based on this, I am thinking of getting Keil as I am just a beginner. So, I believe that I need to buy the 20-pin debug pod (NOT SURE WHICH MODEL) and Keil SW and then can start. Is this all I need to get started?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.