2013-08-11 10:01 AM
I've been looking at some board designs that I've found online, and it looks like some people include an external 8 MHz crystal in a resonator to run their clock. I'm wondering what the benefit of using this external 8 MHz over using the internal 8 MHz crystal in the HSI. Are there any benefits? Thanks for the help in advance.
2013-08-11 2:34 PM
With external crystal you will get better clock accuracy. This may be important, depending on application, for example if you want to use USB, you should use HSE as a clock source.
2013-08-11 3:10 PM
You need external crystals for CAN, ETHERNET and USB to meet specifications for those protocols, as the HSI's RC oscillator is not particularly stable or accurate.
The HSI is also impacted by voltage, temperature, and silicon variations.2013-08-11 4:02 PM
Oh, okay, thanks for the advice. I think I'll keep my external crystal setup then because I'm using USB.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.