2026-04-20 2:30 AM
Hi!
I have a STM32103 processor and I wonder if something bad can occurs if I use an external oscillator to OSC_IN and leave the OSC,_OUT floating. With a ceramic crystal HSE configuration in CubeMX.
I know that the BYPASS clock source is the best HSE configuration for an external source (as I have) because then the OCS_OUT is not oscilating.
But for me, it won't make any difference because my OSC_OUT is floating and not connected to anything. Or will this break after few years of running?
I know that my OSC_OUT have the same oscillations as OSC_IN due to the "wrong" configuration.
Solved! Go to Solution.
2026-04-20 2:35 AM - edited 2026-04-20 2:36 AM
You can leave any output open and nothing will happen, short term or long term.
BUT
remember that unused outputs with some signal inside can be a source of RF noise and that can limit RF compliance.
As a general law, better not to take out unused signals in new design.
2026-04-20 2:35 AM - edited 2026-04-20 2:36 AM
You can leave any output open and nothing will happen, short term or long term.
BUT
remember that unused outputs with some signal inside can be a source of RF noise and that can limit RF compliance.
As a general law, better not to take out unused signals in new design.
2026-04-20 2:39 AM - edited 2026-04-20 2:42 AM
Hello,
@DMårt wrote:I have a STM32103 processor and I wonder if something bad can occurs if I use an external oscillator to OSC_IN and leave the OSC,_OUT floating. With a ceramic crystal HSE configuration in CubeMX.
That statement is a bit ambiguous.
Are you using a crystal (XTAL) or a crystal oscillator (XO)?
If you are using a crystal oscillator (XO) that's the hardware configuration you should adopt in Bypass mode. OSC_IN connected to the oscillator output and OSC_OUT should kept floating.
From the reference manual RM0008:
2026-04-20 2:40 AM
Thank you!
Understand that this might cause bad RF. Luckily, I don't have any RF requirements, only functional requirements.
2026-04-20 2:43 AM
Hi @mƎALLEm
I'm using a XO with a ceramic configuration. But OSC_OUT is floating.
Yes, i know that I should adopt Bypass mode. But in this case it's ceramic/resonator mode.
I hope this won't cause any functional troubles.
2026-04-20 2:45 AM
@DMårt wrote:I don't have any RF requirements
That's not true!
All electronic products need to comply with the relevant EMC regulations wherever they're used/sold.
2026-04-20 2:52 AM
Yes I know, but I don't have been given any such requirements. :)
2026-04-20 2:53 AM
@DMårt wrote:
Hi @mƎALLEm
I hope this won't cause any functional troubles.
No this is what it was suggested in the RM as I stated in my previous post.
2026-04-20 3:03 AM
Yes. But that was for bypass mode. I don't have any bypass configured.
2026-04-20 3:13 AM
@DMårt wrote:I don't have any bypass configured.
Why not?
Bypass is the correct mode to use - so why not just use it?!
You might even be able to use OSC_OUT as an extra GPIO: HSE Bypass mode - Possible use of OSC_OUT as GPIO ... ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.