STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USART PROBLEM

Posted on August 09, 2013 at 20:18Hello, everyone.  I am currently playing around with the USART without standard peripheral lib provided by ST (using CMSIS only) and my code strangely works in one MDK project and does not work in another MDK projec...

ran2 by Associate III
  • 2168 Views
  • 4 replies
  • 0 kudos

AT commands for HTTP

Posted on August 12, 2013 at 09:10Hi all,I am using HILO GSM modem of Sagem. It supports HTTP feature. I am implenting that feature in my device but i am facing problem while using POST and GET commands related to HTTP. I am using AT commands to imp...

manoj23 by Associate II
  • 904 Views
  • 0 replies
  • 0 kudos

Quadrature Encoder Channels

Posted on August 09, 2013 at 20:11I'm working with the STM32F3 Discovery board.  I'm wondering if it is possible to use a timer in encoder interface mode with the signals coming in on Channels 1 and 4.  Do you have to use channels 1 and 2?  Does the...

mattfox by Associate II
  • 1480 Views
  • 2 replies
  • 0 kudos

Current Consumption of STM32L-DISCOVERY in low Power Modes

Posted on August 11, 2013 at 19:23Hi, I am using the STM32L-DISCOVERY evaluation board, and I made JP1 off as per the below instructions from the evaluation board user manual:  JP1 OFF: the STM32L152 is directly powered, IDD measurement circuit is b...

aa_talaat by Associate II
  • 1087 Views
  • 1 replies
  • 0 kudos

HSI vs. HSE crystals

Posted on August 11, 2013 at 19:01I've been looking at some board designs that I've found online, and it looks like some people include an external 8 MHz crystal in a resonator to run their clock.  I'm wondering what the benefit of using this extern...

mattfox by Associate II
  • 2009 Views
  • 3 replies
  • 0 kudos

GNU gcc toolchain on linux

Posted on August 10, 2013 at 00:33Hi all,I've been playing with different peripheral examples of STM32L-Discovery on MDK-ARM (Keil) environment.  Recently I'd like to move to linux with GNU gcc tool chain.  I had a hard time learning to write a Make...

GPIO_Remap_SWJ_Disable Issue

Posted on August 08, 2013 at 23:20 Hey guy's ! [I'd like to apologize for my bad englisch] I think I've made two mistakes in a row... First, I designed a STM32 Board with the usage of the Pin PA.15 - which is remapped after ...

benedikt by Associate II
  • 2158 Views
  • 2 replies
  • 0 kudos

CMSIS DSP PID Algorithm and 1.15 format

Posted on August 10, 2013 at 04:51Hello, I am having a problem with CMSIS DSP. the state variables are represented in 1.15 format.I want to control the speed of a motor using PID algorithm.The minimum value of the PWM duty Cycle is 500 and it Maximu...

STM32W108xx IRQC configuration

Posted on August 06, 2013 at 19:20 Hello all, I'm working on STM32W108xx & interfacing a sensor whose interrupt pin connected to the PB7, IRQC pin. How to configure this pin for the following handler ? void EXTIC_IRQHandler( void ) ...

harinath by Associate III
  • 1506 Views
  • 3 replies
  • 0 kudos

How to unlock SWD on STM32F0?

Posted on August 09, 2013 at 10:15Hi, I accidentally configured USART2 to pins PA14 and PA15 with PA14 being also SWCLK. Now I can't upload code anymore. I read about putting the MCU into bootloader mode by setting BOOT0 to Vdd. But this doesn't wor...

mmensch by Associate II
  • 2505 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.