2020-08-26 11:43 PM
Hi there
I am trying to configure a GPS receiver chip (MAX2769C) with an stm32f446re MCU using SPI in half duplex master mode. The chip is expecting a 32 bit word (4 bits address and 28 bits data). This is on page 21 of the attached datasheet.
It's my first time asking a question on this platform. Thank you in advance!
Solved! Go to Solution.
2020-08-27 7:04 AM
> My first question is how can I transmit a 32 bits word when the maximum bits format that cubemx allows is 16 bits transfer.
You send multiple bytes while holding CS low.
> My second problem is that, I have to generate a clock of exactly 16,384 MHZ to feed the MAX2769C chip (this is not the data clock SCK of the SPI). So I selected MCO1 in cubemx and played around with clock configuration until I got 16.384 MHZ. How is this going to affect the SPI speed?
SPI speed is selected by the relevant peripheral bus speed along with the SPI prescaler.
2020-08-27 7:04 AM
> My first question is how can I transmit a 32 bits word when the maximum bits format that cubemx allows is 16 bits transfer.
You send multiple bytes while holding CS low.
> My second problem is that, I have to generate a clock of exactly 16,384 MHZ to feed the MAX2769C chip (this is not the data clock SCK of the SPI). So I selected MCO1 in cubemx and played around with clock configuration until I got 16.384 MHZ. How is this going to affect the SPI speed?
SPI speed is selected by the relevant peripheral bus speed along with the SPI prescaler.
2020-08-27 8:11 AM
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.