STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750 driving a WS2812B

Hello, I'm looking to use Timer and DMA to drive a WS2812B LED with a STM32H7. TIM8 Ch2 is connected to the LED. I would like to explain what I understand so that its clear and I can get it working.A half word transfer from a memory location to the C...

PNare by Associate III
  • 1008 Views
  • 0 replies
  • 0 kudos

Noise on the 3.3 volt line.

I have a photo interrupter attached to an interrupt port powered by the 3.3. volt supply.Every now and then, there is a burst of activity on the 3,3 volt line which cause havoc on the interrupt line.img_0933 shows the output of the photo interrupter ...

JMazu.1 by Associate III
  • 2125 Views
  • 1 replies
  • 0 kudos

RM0316 ('F303) typos

1) Index contains SYSCFG_MEMRMP but there's no such register in 'F3032) in 5 figures' caption, AUTODLY is mentioned, but there's no such bit, the correct name is AUTDLY (without "O", bit 14 of ADCx_CFGR).JW

Resolved! Performance characteristics of SDRAM on STM32F7508-DISCO board

Below is my benchmarking of multply-accumulate performance on contiguous memory blocks on the STM32F7508-DK board for three different types of memory (on-chip SRAM, external SDRAM managed by the FMC, and QSPI-connected NOR flash):The horizontal axes ...

0693W000002lEueQAE.png
GSpre.1 by Associate III
  • 5659 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.