2024-11-30 10:56 AM - edited 2024-11-30 11:45 AM
I am trying to add 5 to the received number but I can't figure out what am I doing wrong.
This is the code from Keil
uint8_t receivedNumber;
uint8_t newNumber;
while(1){
if(HAL_UART_Receive_IT(&huart2,(uint8_t *)&receivedNumber,sizeof(receivedNumber))==HAL_OK)
{
int newNumber=receivedNumber+5;
HAL_UART_Transmit(&huart2,(uint8_t *)&newNumber,sizeof(newNumber),1000);
}
}
When it receives 1,2,3 or 4, it transmits 6,7,8,9 (as expected). When it receives 5 it transmits a " : " and when it receives 11,21,37 or 42, it transmits 66,76,8< and 97.
Edit:5,6,7,8 to 6,7,8,9
2024-11-30 11:39 AM
Welcome @222student, to the community!
Please read through the coding of characters again (keyword ASCII table). What you are receiving are ASCII characters that cannot be readily calculated.
Incidentally, "5" is not an expected output if you have received "1" and add 5 - is it?
In any case, the (ASCII) character "1" is encoded in binary 0x31. If you add 5, you get 0x36, which corresponds to the character "6" in the ASCII table. However, if you receive, for example, the character "5" with the ASCII equivalent of 0x35, your calculation results in 0x3A, which stands for the character ":".
You must therefore pay attention to WHAT you are receiving and how it is to be INTERPRETED.
Regards
/Peter
2024-11-30 11:48 AM
Thank you so much for the reply, I will look into it.
And yeah, I meant "6,7,8,9" not "5,6,7,8"
2024-11-30 12:48 PM
Perhaps ponder how integer number space vs ASCII works.
Look at sscanf() and sprintf()
Look at atoi() and itoa()
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.