2022-05-03 2:55 AM
To reduce latency time of interruptions.
Based on the same thing but in stm32f0 devices
Solved! Go to Solution.
2022-05-03 2:56 AM
In main.c
/* USER CODE BEGIN PD */
#define VECTOR_TABLE_SIZE (67 + 1 + 13 +9)//67 positive vectors, 0 vector, and 13 negative vectors (and extra 9 i dont know why)
/* USER CODE END PD *//* USER CODE BEGIN PV */
volatile uint32_t __attribute__((section(".ram_vector,\"aw\",%nobits @"))) ram_vector[VECTOR_TABLE_SIZE];
extern volatile uint32_t g_pfnVectors[VECTOR_TABLE_SIZE];
/* USER CODE END PV *//* USER CODE BEGIN 1 */
RCC->CR |= RCC_HSI_ON; // early enable to ensure clock is up and running when it comes to usage
for (uint32_t i = 0; i < VECTOR_TABLE_SIZE; i++) {//copy vector table
ram_vector[i] = g_pfnVectors[i];
}
/* USER CODE END 1 */In system_stm32f1xx.c, uncomment the #define USER_VECT_TAB_ADDRESS
and #define VECT_TAB_SRAM
#define USER_VECT_TAB_ADDRESS */
#if defined(USER_VECT_TAB_ADDRESS)
/*!< Uncomment the following line if you need to relocate your vector Table
in Sram else user remap will be done in Flash. */
#define VECT_TAB_SRAM
#if defined(VECT_TAB_SRAM)
#define VECT_TAB_BASE_ADDRESS SRAM_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x08004800 /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#endif /* VECT_TAB_SRAM */
#endif /* USER_VECT_TAB_ADDRESS */In the linker script (.ld)
.fini_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
. = ALIGN(4);
} >FLASH
/*javi*/
/*https://community.st.com/s/question/0D53W00000trgpiSAA/how-to-boot-to-random-address-without-vecttaboffset-stm32f072*/
/* redirected vector must go to top of the RAM */
.ram_vector :
{
*(.ram_vector)
} >RAM
/*javi*/
2022-05-03 2:56 AM
In main.c
/* USER CODE BEGIN PD */
#define VECTOR_TABLE_SIZE (67 + 1 + 13 +9)//67 positive vectors, 0 vector, and 13 negative vectors (and extra 9 i dont know why)
/* USER CODE END PD *//* USER CODE BEGIN PV */
volatile uint32_t __attribute__((section(".ram_vector,\"aw\",%nobits @"))) ram_vector[VECTOR_TABLE_SIZE];
extern volatile uint32_t g_pfnVectors[VECTOR_TABLE_SIZE];
/* USER CODE END PV *//* USER CODE BEGIN 1 */
RCC->CR |= RCC_HSI_ON; // early enable to ensure clock is up and running when it comes to usage
for (uint32_t i = 0; i < VECTOR_TABLE_SIZE; i++) {//copy vector table
ram_vector[i] = g_pfnVectors[i];
}
/* USER CODE END 1 */In system_stm32f1xx.c, uncomment the #define USER_VECT_TAB_ADDRESS
and #define VECT_TAB_SRAM
#define USER_VECT_TAB_ADDRESS */
#if defined(USER_VECT_TAB_ADDRESS)
/*!< Uncomment the following line if you need to relocate your vector Table
in Sram else user remap will be done in Flash. */
#define VECT_TAB_SRAM
#if defined(VECT_TAB_SRAM)
#define VECT_TAB_BASE_ADDRESS SRAM_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x08004800 /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#endif /* VECT_TAB_SRAM */
#endif /* USER_VECT_TAB_ADDRESS */In the linker script (.ld)
.fini_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
. = ALIGN(4);
} >FLASH
/*javi*/
/*https://community.st.com/s/question/0D53W00000trgpiSAA/how-to-boot-to-random-address-without-vecttaboffset-stm32f072*/
/* redirected vector must go to top of the RAM */
.ram_vector :
{
*(.ram_vector)
} >RAM
/*javi*/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.