STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446 how to use rotary encoder with timer?

I have an application I am converting from another processor to a STM32F446 board. The application uses a rotary encoder to detect counts and direction.I have looked at several videos online on how to use a timer for rotary encoder purposes. I'm begi...

USART1 doesn't communicate using HSE; worked with HSI

Hello, I am new to the ST platform.I actually work with a nucleo144, and i was trying to work with bluetooth hc-06, the problem is that USART1 doesn't communicate with the board when I use HSE in the clock configuration, but it worked when I use HSII...

AAAZO.1 by Associate II
  • 1850 Views
  • 2 replies
  • 0 kudos

Timer1 MOE and breakpoints

I am using an STM32F4 micro using TIM1_CH1 and CH2 outputs to create a communications signal with compare outputs. The first bit that I am outputting is wrong, so I would like so set a breakpoint to see what is going on. BUT, when I check the timer c...

gahelton1 by Associate III
  • 1259 Views
  • 1 replies
  • 0 kudos

Why measured pulse width using TIMER accumulates error as pulse width increases? (understanding inaccuracies in TIMER)

Dear All,Board: Nucleo - H745ZI-QWhat am I trying to do ?I am trying to measure pulse width of an signal using counter mode of timer 2, as accurately as possible. The input pulse width varies from 1 us to 1000 us.What have I done?I configure the Tim...

sarojj7 by Associate III
  • 3090 Views
  • 6 replies
  • 0 kudos

B-L475E-IOT01A Flash Erase & Write

I want to work on flash with B-L475E-IOT01A1.​After flash erase operation, flash write operation is performed, and memory is being checked through debugging.​On other boards, flash erase operation changed the memory in that location to the "?" mark, ...

GKIM.4 by Associate II
  • 769 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.