2022-05-03 12:51 AM - last edited on 2025-04-30 7:35 AM by Andrew Neil
Hello, I am new to the ST platform.
I actually work with a nucleo144, and i was trying to work with bluetooth hc-06, the problem is that USART1 doesn't communicate with the board when I use HSE in the clock configuration, but it worked when I use HSI
In my project I can't use HSI, do you have any suggestions please ?
2022-05-03 3:39 AM
Welcome, @AAAZO.1, to the community!
The HSE can only be used if:
Does it answer your question?
Regards
/Peter
2022-05-03 4:34 AM
On a Nucleo board the HSE clock can come from the STLINK, if it is not populated with a crystal.
But you have to consult the schematics of the board, on some Nucleo there is a solder bridge to add for this functionality.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.