2024-05-26 10:38 AM
I’m using CubeIDE, which lets me configure a timer to trigger a DMA request triggered by an output compare that transfers that timer's value to memory. I want to modify the generated code such that a separate timer’s value is sent to memory instead.
Within the HAL_TIM_OC_Start_DMA function, HAL_DMA_Start_IT is called, (??) which seems to be where the to\from addresses are established. I’m hoping I can modify this call to reference the memory location of another timer’s CNT value…but I’m not certain if its as simple as modifying a single call. I’m up against other anomalous behavior, so I’m not sure if this approach works. Can it?
Solved! Go to Solution.
2024-06-21 12:53 PM
Changing the CPAR and CMAR DMA registers manually accomplishes this.
2024-05-27 9:47 AM
Hello @KHarb.1,
In HAL_DMA_Start_IT, this parameter (&TIMx->CCR1) is the source address, which you would change to the address of the other timer's CNT register.
I personally didn't try this, but I think it should work
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-21 12:53 PM
Changing the CPAR and CMAR DMA registers manually accomplishes this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.