cancel
Showing results for 
Search instead for 
Did you mean: 

cannot configure trigger source for second HRTIM

xiaowenbin
Associate

Two independent outputs have been configured in HRTIM, but the trigger source for the second output cannot be set, indicating that it must be 0.

a9befdac9907205fe41e342ccfba9e20.png

fe07a2d7fb45db1e5fedefef7fad561b.png

 HRTIM中已经设置了两路独立输出,第二路无法设置触发源,提示必须是0

Two independent outputs have been configured in HRTIM, but the trigger source for the second output cannot be set, indicating that it must be 0.

1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hello @xiaowenbin 

Thank you for posting!

This is a known issue and has been already reported to dedicated team as discussed under this thread: Solved: HRTIM configuration when updated to 6.16.1 CubeMX - STMicroelectronics Community

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.