2023-04-26 7:12 PM
I use stm32h745i-disco for work, and want to use dual core system. one for lvgl display, and the other for pn532 rfid, which is needed to communicate each other. anyone have experience about this? pls help
2023-04-27 4:43 AM
Hello,
I invite you to read the AN5617- STM32H745/755 and STM32H747/757 lines inter-processor communications.
If it does answer your question, please click on "Select as best" this answer.
2023-05-09 1:24 AM
Hello, i have read the document but still confused. Can i send some data bytes from cm7 to cm4 using IPC?
2023-05-09 1:36 AM
Hello,
Indeed you can share data between the two cores. You can also refer to the examples provided by STM32CubeH7 package under the path \Projects\STM32H745I-DISCO\Applications\OpenAMP
Also refer to the oscilloscope demo X-CUBE-H7DC-APP.
2023-05-09 3:00 AM
They share a common view of some RAM regions and you can signal via HSEM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.