2023-02-17 2:13 AM
2023-02-17 2:38 AM
The frecuency of the pulses?
why dont you use a proper PWM timer
2023-02-17 2:39 AM
how i can generate the pulse with pwm timer on time-10 us and off time 1 second
2023-02-17 2:42 AM
on time -10 micrsecond,off time -100 miliseconds
2023-02-17 5:15 AM
??? your first is 1Hz freq second is 10Hz explain what you need....
special PWMs you can create with master slave tim or DMA circular ...
2023-02-17 6:12 AM
@MM..1 I believe he is a chatGPT bot using a human's forum.
Machines are asking the questions now
2023-02-17 8:43 AM
HOUUOU SKYNET
2023-02-17 8:51 AM
Communicate which STM32 you are talking about here. What frequency?
Does it have any 32-bit TIM ?
>>on time -10 microseconds, off time -100 milliseconds
9.9990000999900009999 Hz ??
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.