STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H723 RAM configuration

Hey there,I am trying to replace an STM32F767 with an H723ZGT Nucleo Board. The projects uses a lot of heap - in the predefined memory configuration there is not enough place in the RAM_D1 sector. What do I need to do for changing the available RAM s...

PUrsu.1 by Associate II
  • 4968 Views
  • 4 replies
  • 0 kudos

Resolved! Incorrect interrupt firing for stm32f4 CAN2

I have not been able to get CAN2_RX0_IRQ or CAN3_RX0_IRQ to fire. CAN1_RX0_IRQ works as expected. It appears that rather than the CAN IRQs firing, the WWDG interrupt is going off for CAN2_RX0 and the DMA1_Stream0 is going off for CAN3_RX0. Neither th...

KRott.1 by Associate II
  • 2858 Views
  • 4 replies
  • 1 kudos

Resolved! STM32H743 kein CAN-Datenempfang mit 1MBit

We have a project which reads CAN data on both FDCAN ports. Bitrate 500 kBit is working perfectly, but with 1 MBit no data can be read. PIN-Speed = HIGH (also tried MEDIUM and VERY_HIGH, but no change)CAN-Clock = 80 MHzWe already tried CAN Bittiming ...

GS1 by Senior III
  • 1280 Views
  • 1 replies
  • 0 kudos

Resolved! The timing for reading the ADC with DMA seems way too long. I calculate just under 36 us to read 8 ADC channels with a STM32L443CCT running at 64 MHz.

I am trying to trigger every millisecond, or 1000 microseconds, but my counters in the interrupt are seeing 167 interrupts per second as opposed to the expected 1000 interrupts per second.I am reading 6 channels with a sample rate of 92.5 clocks per ...

KiptonM by Lead
  • 7071 Views
  • 8 replies
  • 0 kudos

STM32F103 not programming

Hello i am working on a project which is based on stm32f103c8t6 mcu.i face a issue while programming some of these microcontrollers.sometimes some microcontrollers are programmed perfectly while some start giving errors(see attachment).while going th...

ASakp.1 by Associate II
  • 7224 Views
  • 8 replies
  • 1 kudos

Can I put read/write variables in DTCM, when DCache enabled?

If DCache is enabled how then can I update a variable (I think DMA + MDMA) and after processing get results to a peripheral e.g. DAC (again MDMA?)?Do I need to clear cache?Will I still have the speed advantage of caching?I am struggling how to get d...

leon64 by Associate II
  • 8629 Views
  • 17 replies
  • 0 kudos

Resolved! Cannot cofigure the ADC on STM32L431KB. ADEN always set to 1.

Hi,I am having trouble configuring the ADC on my STM32L431KB. The calibration procedure appears to go well until it gets to the step where the program waits for the calibration to finish. It is never able to finish. I think the problem may be related...

NMill.3 by Associate II
  • 2461 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 PWM Generate when Input Capture Update Event

Hi, I'm doing a project with STM32F769I-EVAL.In my project, I set Timer 2 Channel 1 to input capture mode, and I made a clock to TIM2 CH1 Pin with Function Generator. And Timer 5 Channel1 to PWM Generation CH1 to make a PWM.I calculate frequency of i...

ELee.9 by Associate II
  • 2171 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.