2023-04-18 12:06 PM
2023-04-18 12:55 PM
84M / 874 = 96,11 so...
84M / 437 = 192,22 - 0,1% from 192 . nobody can hear this , so whats the problem?
2023-04-18 2:22 PM
Which STM32?
No perfect soution for these numbers. You can dither, but it depends on application if that is acceptable.
If this is auto application, you should've started with a different crystal.
JW
2023-04-18 10:37 PM
Which STM32 are you using? Maybe you can do something with the PLL?
Or - also depending on the STM32 - use another input for timer clock / the extra I2S clock input.
Otherwise I agree to the above, especially: choose another crystal.
2023-04-19 12:22 AM
Wrong question. The correct one should be: how to get 192 kHz on my microcontroller. The answer is simple - set the main clock to be a multiple of 192 kHz, like 72 MHz. (72000000 / 192000 = 375).
2023-04-19 2:56 AM
Haha yes sure, if only life was so simple. Commercial applications use the lowest cost MCU because business is competitive, our application is real-time, so we can't afford to degrade performance that much, but thanks
2023-04-19 11:32 PM
20% is not much. It doesn't look like a good practice to rely on just 20% performance difference in an application.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.