2021-05-19 9:15 AM
Hello, i'm using STM32G071RB and i need to write on the Flash Memory.
i check if i have wrote on it before. If i did, i try erase the page to re-write. At this point, i just get a HAL_ERROR of the function HAL_FLASHEx_Erase(&EraseInitStruct, &PageError).
i'm doing this:
#define FLASH_USER_START_ADDR 0x08000000
#define USEDPAGES ((uint8_t) 64)
HAL_FLASH_Unlock(); //Unlock memory write permission
FLASH_EraseInitTypeDef EraseInitStruct;
/**Define Erase Struct**/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Page = FLASH_USER_START_ADDR;
EraseInitStruct.NbPages = USEDPAGES;
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK){//Erase Pages
printf("Fail Init Erasing\n");
return 0;
}
i did the same funtions with stm32f0 and i had no troubles with it
2021-05-19 9:22 AM
> #define FLASH_USER_START_ADDR 0x08000000
> EraseInitStruct.Page = FLASH_USER_START_ADDR;
It needs a page number, not an address.
See an example here:
Also in the code:
/**
* @brief FLASH Erase structure definition
*/
typedef struct
{
uint32_t TypeErase; /*!< Mass erase or page erase.
This parameter can be a value of @ref FLASH_Type_Erase */
uint32_t Banks; /*!< Select bank to erase.
This parameter must be a value of @ref FLASH_Banks
(FLASH_BANK_BOTH should be used only for mass erase) */
uint32_t Page; /*!< Initial Flash page to erase when page erase is enabled
This parameter must be a value between 0 and (FLASH_PAGE_NB - 1) */
uint32_t NbPages; /*!< Number of pages to be erased.
This parameter must be a value between 1 and (FLASH_PAGE_NB - value of initial page)*/
} FLASH_EraseInitTypeDef;
2021-05-20 5:40 AM
Hi @FVarg.1 ,
Please refer to the FLASH_EraseProgram example under directory STM32Cube_FW_G0_V1.4.0\Projects\NUCLEO-G071RB\Examples\FLASH of the STM32CubeG0.
Best Regards,
Ons.
Note: If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.