STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 HAL_SAI_Receive() in ISR gets stuck.

Hi, i'm trying to get a value from a microphone using HAL_SAI_Receive() in blocking mode. I'm trying to write a program that receives a value from the mic connected to the SAI block. The HAL_SAI_Receive() is called in an ISR but when the program is r...

RBamf.1 by Associate III
  • 2438 Views
  • 6 replies
  • 0 kudos

Resolved! Web page inconsistency STM32F7x5 caching

https://www.st.com/en/microcontrollers-microprocessors/stm32f7x5.htmlTop of page talks about I/D cache being 4K+4Kon sub pages becomes 16K + 16K for 32K total https://www.st.com/en/microcontrollers-microprocessors/stm32f765vi.html 

0693W00000AP4BhQAL.jpg 0693W00000AP4FoQAL.jpg

Resolved! Would it be possible to run code that is partly written in internal flash and partly written in external flash?

Hi everyone!Quick question: this is my platform.STM32F4 main controllerexternal QSPI flashI'm currently using FreeRTOS with TouchGFX so the external flash stores the graphical resources. In case I run out of memory, could I run some of the code (the ...

Auloedus by Associate II
  • 2335 Views
  • 4 replies
  • 0 kudos

Resolved! Nucleo-F042k Doesn't Seem to Function

I just received (about 4 hours ago) 2 Nucleo-F042K6 boards. I tried to a LED blinker program but both units hang in the Clock Configuration routine. Strange that both units exhibit the same behavior. I'm wondering if I missed something. I used C...

DIngr.1 by Associate II
  • 1709 Views
  • 2 replies
  • 0 kudos

DMA burst mode dont work correctly

I want to generate an arbitrary wave form on channel1 and channel2 of timer1. I use dma burst mode and other:MCU: STM32f401CCU6Frequency: 84 MhzTIM1 PSC: 84-1TIM1 Counter Mode: Center aligned mode 1TIM1 RCR: 1TIM1 ARR: 1000TIM1 frequency is 500 and t...

0693W00000AP05BQAT.jpg 0693W00000AP05kQAD.gif 0693W00000AP06TQAT.gif
eqbal by Associate II
  • 2135 Views
  • 3 replies
  • 0 kudos

HAL_ERROR when i try to erase the flash memory

Hello, i'm using STM32G071RB and i need to write on the Flash Memory.i check if i have wrote on it before. If i did, i try erase the page to re-write. At this point, i just get a HAL_ERROR of the function HAL_FLASHEx_Erase(&EraseInitStruct, &PageErro...

FVarg.1 by Associate
  • 3390 Views
  • 2 replies
  • 0 kudos

nBOOT1 pin on STM32L073RZT6

Dear ST Community,I am now designing a PCB with the STM32L073RZT6. Could you please advise where the BOOT1 pin is located?Inside the datasheet, the only thing that I found is the statement:Boot modes At startup, BOOT0 pin and nBOOT1 option bit are us...

VMeto.1 by Associate II
  • 2002 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.