2018-05-14 9:14 AM
.
2018-05-17 6:56 AM
I AM using STM32479I EVAL BOARD and Here is the clock configuration generated by CubMX
void SystemClock_Config(void)
{RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInitStruct; HAL_StatusTypeDef ret = HAL_OK;/**Configure the main internal regulator output voltage
*/ __HAL_RCC_PWR_CLK_ENABLE();__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 15; RCC_OscInitStruct.PLL.PLLN = 144; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 5; RCC_OscInitStruct.PLL.PLLR = 2; ret = HAL_RCC_OscConfig(&RCC_OscInitStruct);if(ret != HAL_OK)
{ Error_Handler(); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SDIO|RCC_PERIPHCLK_CLK48;
PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48CLKSOURCE_PLLQ; PeriphClkInitStruct.SdioClockSelection = RCC_SDIOCLKSOURCE_CLK48; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0);}2018-05-23 8:39 PM
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0); // Least priority, worst possible setting for a value you expect to tick under interrupt context everywhere else/* Set Systick interrupt in high priority for HAL_Delay() */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0); // Use this to ensure it firesThe HAL_NVIC_SetPriorityGrouping() should create 16 levels of preemption
/**
* @brief This function configures the source of the time base: * The time source is configured to have 1ms time base with a dedicated * Tick interrupt priority. * @note This function is called automatically at the beginning of program after * reset by HAL_Init() or at any time when clock is reconfigured by HAL_RCC_ClockConfig(). * @note In the default implementation, SysTick timer is the source of time base. * It is used to generate interrupts at regular time intervals. * Care must be taken if HAL_Delay() is called from a peripheral ISR process, * The SysTick interrupt must have higher priority (numerically lower) * than the peripheral interrupt. Otherwise the caller ISR process will be blocked. * The function is declared as __weak to be overwritten in case of other * implementation in user file. * @param TickPriority Tick interrupt priority. * @retval HAL status */__weak HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority){ /*Configure the SysTick to have interrupt in 1ms time basis*/ HAL_SYSTICK_Config(SystemCoreClock/1000);/*Configure the SysTick IRQ priority */
HAL_NVIC_SetPriority(SysTick_IRQn, TickPriority ,0);/* Return function status */
return HAL_OK;}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.