2017-12-18 11:18 AM
Hi Everyone.
I recently updated my SW4STM32 IDE when prompted to do so from a pop up, and I'm now seeing its taking forever to compile a project. For example I cleaned one of my
mailto:STM#@F0
Adafruit LCD shield demo programs and then rebuilt it with the following stats finally displayed via the console view.06:07:06 Build Finished (took 1m:46s.283ms), this is forever?
It was going through building each file one by one taking at least a second or so on each file. Is this something someone else is experiencing, can I fix this somehow?
EDIT: Also making a trivial code change produced this.
06:20:51 Build Finished (took 4s.363ms)
Thanks
mb
2018-05-23 9:10 PM
Hi
B.M.002
,What was the code change you made to speed up compilation ?
My full project is taking 15 minutes to compile for no special reason.Thanks a lot
AlexWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.