2021-07-29 10:52 PM
Hello,
In my project I must use extended CANBUS protocol on STM32L496 and STM32H743 microcontrollers.
Does any one have example how to use it ? None on STM examples comes with extended canbus demo, googling also did not give any results.
I have working setup for regular canbus
Any examples would be welcome !
Thank you
2021-07-29 11:32 PM
Hi,
Please show us some actual code as a first step to help you.
Can you tell us what do you mean by "extended CAN bus protocol" ?
Best regards.
2021-07-30 12:01 AM
It is 2.0B Version. Nearly all examples or projects on the internet use 2.0A version.
Its extended address space can bus protocol.
This is typical 2.0A implementation:
FDCAN_HandleTypeDef hfdcan;
FDCAN_RxHeaderTypeDef RxHeader;
uint8_t RxData[8];
FDCAN_TxHeaderTypeDef TxHeader;
uint8_t TxData[8];
static void FDCAN_Config(void)
{
FDCAN_FilterTypeDef sFilterConfig;
/* Bit time configuration:
fdcan_ker_ck = 40 MHz
Time_quantum (tq) = 25 ns
Synchronization_segment = 1 tq
Propagation_segment = 23 tq
Phase_segment_1 = 8 tq
Phase_segment_2 = 8 tq
Synchronization_Jump_width = 8 tq
Bit_length = 40 tq = 1 µs
Bit_rate = 1 MBit/s
*/
hfdcan.Instance = FDCANx;
hfdcan.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan.Init.AutoRetransmission = DISABLE;
hfdcan.Init.TransmitPause = DISABLE;
hfdcan.Init.ProtocolException = ENABLE;
hfdcan.Init.NominalPrescaler = 0x1; /* tq = NominalPrescaler x (1/fdcan_ker_ck) */
hfdcan.Init.NominalSyncJumpWidth = 0x8;
hfdcan.Init.NominalTimeSeg1 = 0x1F; /* NominalTimeSeg1 = Propagation_segment + Phase_segment_1 */
hfdcan.Init.NominalTimeSeg2 = 0x8;
hfdcan.Init.MessageRAMOffset = 0;
hfdcan.Init.StdFiltersNbr = 1;
hfdcan.Init.ExtFiltersNbr = 0;
hfdcan.Init.RxFifo0ElmtsNbr = 1;
hfdcan.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan.Init.RxFifo1ElmtsNbr = 0;
hfdcan.Init.RxBuffersNbr = 0;
hfdcan.Init.TxEventsNbr = 0;
hfdcan.Init.TxBuffersNbr = 0;
hfdcan.Init.TxFifoQueueElmtsNbr = 1;
hfdcan.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
if (HAL_FDCAN_Init(&hfdcan) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/* Configure Rx filter */
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x321;
sFilterConfig.FilterID2 = 0x7FF;
if (HAL_FDCAN_ConfigFilter(&hfdcan, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/* Start the FDCAN module */
if (HAL_FDCAN_Start(&hfdcan) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
/* Prepare Tx Header */
TxHeader.Identifier = 0x321;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_8;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
}
void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
if((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != RESET)
{
/* Retreive Rx messages from RX FIFO0 */
if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
/* Reception Error */
Error_Handler();
}
/* Display LEDx */
if ((RxHeader.Identifier == 0x321) && (RxHeader.IdType == FDCAN_STANDARD_ID) && (RxHeader.DataLength == FDCAN_DLC_BYTES_2))
{
// LED_Display(RxData[0]);
ubKeyNumber = RxData[0];
}
if (HAL_FDCAN_ActivateNotification(hfdcan, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
}
}
#define FDCANx FDCAN1
#define FDCANx_CLK_ENABLE() __HAL_RCC_FDCAN_CLK_ENABLE()
#define FDCANx_RX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
#define FDCANx_TX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
#define FDCANx_FORCE_RESET() __HAL_RCC_FDCAN_FORCE_RESET()
#define FDCANx_RELEASE_RESET() __HAL_RCC_FDCAN_RELEASE_RESET()
/* Definition for FDCANx Pins */
#define FDCANx_TX_PIN GPIO_PIN_9
#define FDCANx_TX_GPIO_PORT GPIOB
#define FDCANx_TX_AF GPIO_AF9_FDCAN1
#define FDCANx_RX_PIN GPIO_PIN_8
#define FDCANx_RX_GPIO_PORT GPIOB
#define FDCANx_RX_AF GPIO_AF9_FDCAN1
/* Definition for FDCANx's NVIC IRQ and IRQ Handlers */
#define FDCANx_IRQn FDCAN1_IT0_IRQn
#define FDCANx_IRQHandler FDCAN1_IT0_IRQHandler
void HAL_FDCAN_MspInit(FDCAN_HandleTypeDef* hfdcan)
{
GPIO_InitTypeDef GPIO_InitStruct;
RCC_PeriphCLKInitTypeDef RCC_PeriphClkInit;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO TX/RX clock */
FDCANx_TX_GPIO_CLK_ENABLE();
FDCANx_RX_GPIO_CLK_ENABLE();
/* Select PLL1Q as source of FDCANx clock */
RCC_PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_FDCAN;
RCC_PeriphClkInit.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL;
HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphClkInit);
/* Enable FDCANx clock */
FDCANx_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* FDCANx TX GPIO pin configuration */
GPIO_InitStruct.Pin = FDCANx_TX_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = FDCANx_TX_AF;
HAL_GPIO_Init(FDCANx_TX_GPIO_PORT, &GPIO_InitStruct);
/* FDCANx RX GPIO pin configuration */
GPIO_InitStruct.Pin = FDCANx_RX_PIN;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Alternate = FDCANx_RX_AF;
HAL_GPIO_Init(FDCANx_RX_GPIO_PORT, &GPIO_InitStruct);
/*##-3- Configure the NVIC #################################################*/
/* NVIC for FDCANx */
HAL_NVIC_SetPriority(FDCANx_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(FDCANx_IRQn);
}
void FDCANx_IRQHandler(void)
{
HAL_FDCAN_IRQHandler(&hfdcan);
}
2021-07-30 3:20 AM
Great. So you want to use extended ID.
I'm not using HAL, but if your IDE is eclipse based (like Atollic TrueStudio or STM CubeIDE), you can CTRL+CLICK on any constant or variable and you will be redirected to its definition.
In your case I would CTRL+CLICK on FDCAN_STANDARD_ID (line 52 and 79) to see if FDCAN_EXTENDED_ID exists or not (I think it does). Replace all occurence of FDCAN_STANDARD_ID with its extended equivalent in the above code. Line 34 should be set to 0 (no standard ID filters) and line 35 to 1 (we want to filter the extended IDs).
The last step is too change the IDs to the actual value you want to use.
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.