2018-06-20 12:16 AM
Hey there,
I have a development board that includes STM32F091CC. After write my code i successfully build it but when i try to debug in Atollic TrueStudio(Eclipse based IDE) it i have an error messages that in attached.
Note : When i use ST LINK Utility i successfully connect and program my mcu but in IDE i can not.
Error in initializing ST-Link device. Reason:(4) No device found on target.
In my debug configuration i try to debug in Embedded C/C++ Application and my parameters just like that. Can you help me to figure out the problem.
Thanks.
#eclipse-debug #debug-issue #debug_mode #debug2018-08-10 10:01 AM
Some settings issue or fiddling with debug pins, or low power modes.
Check firmware version
Check drivers/scripts
Connect under reset, or with BOOT0 High
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.