2018-06-05 5:20 AM
Hello,
I'm trying to communicate between a STM32F746G Discovery Board and a Powersupply (over PMBus).
While doing so i realized that the SCL wire is kept low after the ACK Bit of the Powersupply.To eleminate possible mistakes on the Powersupply side I switched to a STM32F769 Discovery Board as a slave and used the 'I2C_TwoBoards_ComIT' Preject from the STM32Cube_FW_F7_V1.11.0 on both boards.I only changed the 'I2C_ADDRESS' on line 54 to 0x9A on both boards, the '
I2cHandle.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT' an both (line 110) and set MASTER_BOARD to comment on the STM32F769.the result is still, a low SCL line after the ACK bit.
I tried using HAL_I2C_Master_Transmit() and everything works just as it should i can even write data to the Powersupply.
Any help is welcome.I Added a picture of an oscilloscope showing the BUS.#i2c-example #pmbus #stm32-i2c-smbus2018-08-10 10:06 AM
Sorry, bumping old zombie unanswered threads off my feed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.