2024-08-03 8:25 AM
Hi to all,
I am moving to SPM32CubeIDE on Linux and, as a newby, I encountered a lot of problems.
I started a new empty C++ project and I put all my flies and classes.
I also included syscall.c file (renamed in syscall.cpp) as in it there are _seek(), _read(), ..... routines, but everytime I compile my program I always got:
(.text._close_r+0xc): warning: _close is not implemented and will always fail
(.text._lseek_r+0x10): warning: _lseek is not implemented and will always fail
(.text._read_r+0x10): warning: _read is not implemented and will always fail
(.text._write_r+0x10): warning: _write is not implemented and will always fail
Finished building target: F303.elf
What should I do to make the linker to attach those routines?
Thank you
Freya
2024-08-03 9:20 AM
Those are linker warnings, not errors. They are harmless as long as you don't intend using a file system on the board and you can ignore them.
The messages say what you could do for fixing these warnings: implement the functions. An empty function body will do. Since you are using C++, there is a chance that these functions are already implemented, but in C++, not C. C++ does name mangling and the linker will not find the C++ implmentations unles they are decorated by extern "C".
> as a newby,
Look for known good examples before changing too much. Embedded waters are deep and fierce creatures are living there.
hth
KnarfB
2024-08-03 9:22 AM - edited 2024-08-03 9:25 AM
Hi,
basically the IDE is on C . Just start stm32-project, as c++ , generate code from your MX/ioc .
So dont rename main.c , etc. , generated code files /HAL lib is always C ;
and
> I put all my flies and classes
-- no. Only menu -> import -> file system ... will let the IDE know, this is part of your project. So import your files.
Just from main.c call your C++ ...whatever : my_main.cpp , then you get working project, cpp compiler is called, on your c++ files, other is and will be C.
2024-08-03 10:26 AM
> syscall.c file (renamed in syscall.cpp)
You generally should not be renaming C files to C++ files, especially for low-level system files like this. This mangles the function names so the linker doesn't see them for what they are anymore.
The majority of "C++" projects have a significant number of C files in them. Just an artifact of how the infrastructure grew up.
If you want to create C++ source files, create new ones and launch them from a function call within main().
2024-08-03 11:51 AM
Thank you to all,
the problem is solved. The fil continue to have extension .cpp, but I added before the function declaration extern "C" and now I have no more warnings.
Thank you
Freya
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.