2017-11-14 3:28 AM
Hello ST team
I'm writing to you because I'm working on
STM32F746ZGTx, but I have found the same BUG problem with the SD card in CubeMx version 4.23.0 library Firmware package STM32F7 v1.8.0.Before I was working with CubeMX 4.21.0 and Firmware Package 1.7.0 and the problem with the SD card was solved, now I updated with the new version 4.23.0 and seems the .h and .c files have a lot of changes (for instance the
stm32f7xx_hal_sd.c file
)Please, could you fix the issues?
best
2017-11-14 5:53 AM
Hi
jacinto.juan
,This should be the same issue as reported in
https://community.st.com/0D50X00009XkXvgSAF
.We are already aware of this issue that should be fixed in next release.
Sorry for such inconvenience.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-12-07 2:15 AM
Hello,
Please refer to the following if you have similar issue:
-
https://community.st.com/0D50X00009bMM8bSAG
-
https://community.st.com/0D50X00009XkXg5SAF
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-02-15 2:00 AM
Hi
Jacinto.Juan
,If you are talking about the issue highlighted here
https://community.st.com/0D50X00009bMM8bSAG
, indeed, the correction is available in the current CubeMX release (4.24).Please, update your release with the latest one.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.