2017-11-13 1:26 PM
Where to find the ACIM FOC library for STM32 ? When it will be in the STM32Cubexx ?
2017-11-14 5:40 AM
Hi
Cinelli.Antonio
,Your request is transferred to our CubeMX who can decide if such request may be considered in new tool features.
Thanks for sharing.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-02-15 1:36 AM
Hello,
Are you aware of this library :
http://www.st.com/en/embedded-software/stsw-stm32100.html
?The STM32 PMSM FOC SDK(STSW-STM32100), which includes the PMSM FOC FW library and ST MC Workbench, allows the user to evaluate the STM32 performance in applications driving single or dual Field Oriented Control of 3-phase Permanent Magnet motors (PMSM, BLDC).
You can find the full description on Motor Control Software Development Kit in
.I am pretty sure it will help you.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.