2021-02-11 8:18 PM
I read the ref manual several times but it is still unclear to me. I have a problem with a DMA design that is transferring TIM8_CH1 and TIM8_CH3 to memory using DMA_Channel1 and DMA_Channel2. I am getting a transfer error so am looking at what could cause this.
The timer value is uint32_t and the buffers are both 4-byte aligned. Is this okay? (I think so)
I do not understand the DMAMUX explanation in the ref manual page RM0440, page 384 Table 80. I see TIM8_CH1 is on DMA input request #49 and TIM8_CH3 is on DMA input request #51. How do these map to DMA Channel # on DMA1 and DMA2?
Can TIM8_CH1 and TIM8_CH3 be used respectively on DMA1_Channel1 and DMA1_Channel2. I can't seem to answer this from the ref manual do to my lack of understanding the explanation. The tables for the F303x and L41x are much clearer.
My understanding is a transfer error is caused by a bus fault, such as an illegal address. My destination data buffers are at 0x2000000C and 0x20000034. Are these an issue?
Thanks for any clarification you can offer, much appreciated.
BT
2021-02-13 4:03 AM
Okay, I reduced my code to a minimum that was only running the DMA as described above. With TIM8 running and using capture on CH1 and CH3 I was able to trigger DMA1_CH1 and DMA2_CH2. Incidentally, this is using an external trigger on CH1 and a software trigger on CH3.
Whatever problem I am having in my complete code is not a problem with this Timer/DMA configuration. It still stands the DMAMUX documentation on the STM32G431 really fails compared to other ST devices. With 2127 pages in the Ref Manual they failed to communicate.
2021-03-10 7:07 AM
Hi @BTrem.1 ,
A complementary content to what is already provided in the reference manual regarding DMA request multiplexer is provided in AN5224 (STM32 DMAMUX: the DMA request router).
Depending on the product where this multiplexer is available, this application note explains its features. It explains as well how to properly configure it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.