STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 USART baudrate max rate

Hi allI used STM32F429 connected with LTE module by USART3,but I can only set the baudrate 230600. If I set 460800 or 921600,MCU can't transmit or receive data from LTE.How can I set the baudrate over 230600??void uart_init() { UART3_Handler.Instanc...

YChen.51 by Associate II
  • 2833 Views
  • 4 replies
  • 0 kudos

Trying to setup DMA for I2C on STM32L4R

Hi,I'm trying to set up DMA transfers for I2C sensors on STM32L4R9 MCU.I've followed the documentation and analyzed the HAL implementation, but the DMA channel IRQ handler is never triggered.Here's the specific sequence of steps that I'm performing:F...

MGode by Associate
  • 950 Views
  • 0 replies
  • 0 kudos

WWDG interrupt(EWI) is not getting while writing Flash

Hi ,I am in STM32L071CZ and using window WDG EWI to refresh the WDG counter to avoid RESET.window = 127Counter = 127Prescaler 8Enabling the EWI and reloading the wdg counter in the ISR to avoid the RESET by WWDG.But while writing Flash it seems the W...

SN by Associate II
  • 5100 Views
  • 3 replies
  • 0 kudos

QSPI Problem with AutoPolling with MX25L512 nor flash

Hi,I'm trying to implement Macronix MX25L512 with STM32L476, FATFS and USB MSC.I don't understand why but AutoPolling function timeout.According to the code below, QSPI_Driver_init() is the first function called. QSPI_ResetMemory return QSPI_OK, but ...

ACHAB.1 by Associate
  • 3390 Views
  • 1 replies
  • 0 kudos

Can I join a later workshop?

We (Steven Burck and Haim Kleinman) have prepared the setups for tomorrows workshops, however, Steven is quarantined till next week and won't be able to make it, and Haim will not arrive to the site until 10AM CET. We have a third engineer who was p...

SBurc by Associate II
  • 1388 Views
  • 2 replies
  • 0 kudos

Can someone explain the DMAMUX mapping on the STM32G431?

I read the ref manual several times but it is still unclear to me. I have a problem with a DMA design that is transferring TIM8_CH1 and TIM8_CH3 to memory using DMA_Channel1 and DMA_Channel2. I am getting a transfer error so am looking at what could ...

BTrem.1 by Senior II
  • 1653 Views
  • 2 replies
  • 0 kudos

Register confusion on stm32f401RE

I am having a but of an issue with setting the registers to portA directly using its address.I am doing this for demonstration/learning purposes. I am using the STM32F401RE board.When I read the datasheet it says that GPIO PORT starts on register ->0...

CMcC.1 by Associate II
  • 2630 Views
  • 7 replies
  • 0 kudos

Which MCU supports CSI slave mode?

I want to drive the external sensor to collect images through MCU, and the timing MCU outputs signals in CSI standard format. Which MCU can support this function (MCU acts as a camera)

0693W000007Zq2WQAS.png
Ygu.11 by Associate
  • 1038 Views
  • 1 replies
  • 0 kudos

Board STM32H735G-DK Ordered

Hello,As you have requested, I have ordered the board via ST e-store on March 1st. Also, I have got the order confirmation from ST.Further, when can I expect to receive the news of the seat reservation from ST ?Thank you and with my kind regards,Sue

Sue.Jay by Associate II
  • 2453 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.