2018-01-11 2:54 AM
Under Linux Debian Stretch:
- if I use the shortcut nothing happens
- if I type ./STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammerLauncher,
I have this error message: Error: Could not find or load main class com.st.app.Main
What should I do in order to run Cube Programmer ?
Regards
Cedric
Solved! Go to Solution.
2020-04-15 8:09 PM
It works perfectly for me, thanks!
2020-04-30 7:00 AM
I have followed the downgrade instructions and can now run Cube Programmer on Ubuntu 18.04, but when I start it from the command line, I get:
> /usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammer
jar:file:/usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammerLauncher!/fxml/Config.fxml
java.lang.ClassNotFoundException: com.sun.deploy.uitoolkit.impl.fx.HostServicesFactory
at java.net.URLClassLoader.findClass(URLClassLoader.java:382)
at java.lang.ClassLoader.loadClass(ClassLoader.java:418)
at java.lang.ClassLoader.loadClass(ClassLoader.java:351)
at java.lang.Class.forName0(Native Method)
at java.lang.Class.forName(Class.java:348)
...
Also, I can now connect to STM32WB55.USBDONGLE, but I can't read the memory and the device information is not showing. Whey I googled the above error, it appears it was a bug fixed in a later version of openjfx (There is an existing bug on Mac platform that showDocument() will lead to an illegalAccessException. To workaround this problem an --add-exports option is required, i. e. --add-exports=java.desktop/com.apple.eio=javafx.graphics ) that is not available for Ubuntu 18.04 and I don't know how to apply the fix. I also had udev problems that I hopefully fixed properly. Does anyone have Programmer working for a WB55 dongle on Ubuntu 18.04? Is there any visibility on how to get around these problems? Is it expected that ST will address this or should I look for anothe alternative or just give up on the dongle? Any suggestions are appreciated. Thank you.
2020-04-30 10:17 PM
Got the same issue on Ubuntu 18.04 LTS, installed EVERYTHING as described Oracle JDK + JRE, and openjdk using sudo apt get and by hand.
Even tried compiling a java example using Jfx as per the openjfx :
https://openjfx.io/openjfx-docs/#install-javafx
javac --module-path $PATH_TO_FX --add-modules javafx.controls,javafx.fxml HelloFX.java
The example compiled fine but i tried it many times using sudo and not and the STcube programmer exec keeps failing !!!
/usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammerLauncher
Error: Could not find or load main class com.st.app.Main
Caused by: java.lang.NoClassDefFoundError: javafx/application/Application
JDK/JRE
java -version
java version "11.0.7" 2020-04-14 LTS
Java(TM) SE Runtime Environment 18.9 (build 11.0.7+8-LTS)
Java HotSpot(TM) 64-Bit Server VM 18.9 (build 11.0.7+8-LTS, mixed mode)
echo $JAVA_HOME
/opt/jdk/usr/lib/jvm/jdk-11.0.7
romain@romain-linux:/opt/jdk/usr/lib/jvm/jdk-11.0.7/lib$ sudo update-alternatives --display java
java - auto mode
link best version is /opt/jdk/usr/lib/jvm/jdk-11.0.7/bin/java
link currently points to /opt/jdk/usr/lib/jvm/jdk-11.0.7/bin/java
link java is /usr/bin/java
/opt/jdk/usr/lib/jvm/jdk-11.0.7/bin/java - priority 100
/opt/jdk/javafx-sdk-11.0.2/lib$ ls
javafx.base.jar javafx.media.jar javafx.web.jar libavplugin-ffmpeg-56.so libglassgtk2.so libjavafx_font_freetype.so libjfxmedia.so libprism_sw.so
javafx.controls.jar javafx.properties libavplugin-54.so libavplugin-ffmpeg-57.so libglassgtk3.so libjavafx_font_pango.so libjfxwebkit.so src.zip
javafx.fxml.jar javafx.swing.jar libavplugin-56.so libdecora_sse.so libglass.so libjavafx_font.so libprism_common.so
javafx.graphics.jar javafx-swt.jar libavplugin-57.so libfxplugins.so libgstreamer-lite.so libjavafx_iio.so libprism_es2.so
There you go all proof that everything is done by the book:
1) java home configure
2) java and javac installed
3) ubuntu is configured with the right kit
4) libs from openjfx reside in the JDK lib directory
PLEASE help i think that ubuntu 18 is very mainstream and this should work when the oracle JDK and JRE are installed as per the book and same for the openJFX.
Thanks by advance !
This is really hard to believe that with about 12 years of experience as a developer i cannot get STM32cube to work.
Not a good look and first impression to say the least...
And btw why arent all these instructions about jfx not included in your installer or in a README ?
2020-06-17 6:41 AM
Same behavior here with a Debian 10.
I downgraded openjfx and now when I execute the STM32CubeProgrammer from command line I get the following result:
./STM32CubeProgrammer
Jun 17, 2020 3:29:10 PM javafx.fxml.FXMLLoader$ValueElement processValue
WARNING: Loading FXML document with JavaFX API of version 8.0.121 by JavaFX runtime of version 8.0.111
jar:file:/home/isidre/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammerLauncher!/fxml/Config.fxml
java.lang.ClassNotFoundException: com.sun.deploy.uitoolkit.impl.fx.HostServicesFactory
at java.net.URLClassLoader.findClass(URLClassLoader.java:382)
at java.lang.ClassLoader.loadClass(ClassLoader.java:418)
at java.lang.ClassLoader.loadClass(ClassLoader.java:351)
at java.lang.Class.forName0(Native Method)
at java.lang.Class.forName(Class.java:348)
at com.sun.javafx.application.HostServicesDelegate.lambda$getInstance$0(HostServicesDelegate.java:52)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.HostServicesDelegate.getInstance(HostServicesDelegate.java:45)
at javafx.application.HostServices.<init>(HostServices.java:52)
at javafx.application.Application.getHostServices(Application.java:334)
at com.st.app.Main.start(Main.java:51)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication1$8(LauncherImpl.java:863)
at com.sun.javafx.application.PlatformImpl.lambda$runAndWait$7(PlatformImpl.java:326)
at com.sun.javafx.application.PlatformImpl.lambda$null$5(PlatformImpl.java:295)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.PlatformImpl.lambda$runLater$6(PlatformImpl.java:294)
at com.sun.glass.ui.InvokeLaterDispatcher$Future.run(InvokeLaterDispatcher.java:95)
at com.sun.glass.ui.gtk.GtkApplication._runLoop(Native Method)
at com.sun.glass.ui.gtk.GtkApplication.lambda$null$5(GtkApplication.java:139)
at java.lang.Thread.run(Thread.java:748)
2020-07-04 8:02 AM
You need to start the STM32 Cube Programmer with Oracle Java 8. See https://community.st.com/s/question/0D50X00009q3X4jSAE/stm32cubeprogrammer-for-linux?t=1593874663726 where the same topic is discussed.
2020-08-18 2:33 AM
Possibly one more quick solution found in another thread:
For programmer had to install Liberica / bellsoft-jdk8u265+1-linux-amd64-full.deb
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.