2017-08-21 5:16 AM
I tried to use LL library for stm32f10x without CubeMX ( * @version V1.1.1 * @date: 12-May-2017) and almost immediately found some problems:
1) You can't actually download LL library without CubeMX, even if you don't want to use Cube. That's not a but, that's just irritating.
2) It seems that you can't enable clocking of any periphery because there is no equivalent of RCC_AHBPeriphClockCmd in ll_rcc module.
3) If I enabled GPIO blocking with something like
RCC->APB2ENR |= RCC_APB2ENR_IOPCEN;
and then try to do:RCC->APB2ENR |= RCC_APB2ENR_IOPCEN;
LL_GPIO_InitTypeDef initStruct;
LL_GPIO_StructInit( &initStruct );
initStruct.Mode = LL_GPIO_MODE_OUTPUT_10MHz;
initStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
initStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
initStruct.Pin = LL_GPIO_PIN_9; // that equals 0x04020002
LL_GPIO_Init( GPIOC, &initStruct )
This code will actually init PC.2 to output push-pull.
Why? LL_GPIO_Init does this:
pinpos = POSITION_VAL(GPIO_InitStruct->Pin);
where
#define POSITION_VAL(VAL) (__CLZ(__RBIT(VAL)))
obviously, pinpos will be equal to 1.
Then current pin will be calculated like this:
currentpin = (GPIO_InitStruct->Pin) & (0x00000101U << pinpos);
so currentpint will be equal to 2.
And then
LL_GPIO_SetPinMode(GPIOx, currentpin, GPIO_InitStruct->Mode);
will be called, despite the fact that LL_GPIO_SetPinMode should accept parameters like LL_GPIO_PIN_x.
4) And here we have another 'bug' - all inline functions in header files do not check their arguments with assert_param!
I'm actually startled, how something as simple as this can be broken and not tested?! Or maybe i'm horribly wrong and just using LL library in the wrong way?
2017-08-21 5:53 AM
1. Isn't it bundled with
?2. That's not true, look at the numerous examples at STM32Cube_FW_F1_V1.6.0/Projects/STM32F103RB-Nucleo/Examples_LL
4. Maybe this is deliberate. LL is a lightweight and advanced library, you should know what you are doing. assert_params would use a lot of space if used in every inline function, there was a case when I couldn't use the default debug build of a project with HAL because assert_params use too much flash.
2017-08-21 9:00 AM
1) I can't see a big difference between CubeF1 and CubeMX. I still can't just download the sources of the library, I have to generate a project and install unnecessary software.
2) My bad, haven't looked in the bus.h.
3) That's my main concern here.
4) assert_params are already optional. We need them at the debug stage, we disable them after all stupid bugs are fixed. I would prefer having them everywhere.
2017-08-21 9:16 AM
1) Well there is a big difference. CubeMX is the software, whereas, last time I checked, CubeFx and CubeLx are only the archived library files (with their examples, documentation, etc) without the 'unnecessary software'.
3) I can't look at it right now to try to confirm/deny the bug, maybe somebody else can help.
4) I tend to agree.
2017-08-21 9:30 AM
1) Jeez, you are right! Please excuse my ignorance!
2017-11-30 5:54 PM
3. LL F1 series lib has an error in the configuration function LL_GPIO_Init. You can fix it or do not use. Unfortunately, I just study the library for academic purposes and can not guarantee the working capacity after correction. But you can try written
'>> 8'
in two places:/* Initialize pinpos on first pin set */
pinpos = POSITION_VAL((GPIO_InitStruct->Pin>>8)); /* Configure the port pins */ while ((((GPIO_InitStruct->Pin>>8) & 0x0000FFFFU) >> pinpos) != 0x00000000U)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.