STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bugs in stm32f10x LL library

Posted on August 21, 2017 at 14:16I tried to use LL library for stm32f10x without CubeMX (  * @version V1.1.1  * @date: 12-May-2017) and almost immediately found some problems:1) You can't actually download LL library without CubeMX, even if you don...

amomum by Associate III
  • 3149 Views
  • 5 replies
  • 0 kudos

CubeMX error code generation

Posted on November 07, 2016 at 12:19When regenerating code (previously correctly generated several times) CubeMX displays an error window and deletes an initialization assembler source file which prevents the Eclipse/System Workbench project to buil...

X-NUCLEO-IHM02A1 w/STM32F302R8 Problems

Posted on November 30, 2017 at 23:43I am using a X-NUCLEO-IHM02A1 dual stepper motor driver evaluation board paired with a NUCLEO STM32F302R8 board. My IDE is the System Work Bench for STM32. The motor driver comes with a software package for contai...

Resolved! STM32F746 Discovery Board External SDRAM Address crash

Posted on November 30, 2017 at 17:28Hi, I'm new here.I've started a project using the STM32F746 Discovery board and I've been messing around with the external SDRAM.I copied the initialisation code from the FMC example, and used STM32CubeMX for the ...

stm32l486 sdio

Posted on November 30, 2017 at 21:23Hi I have been trying to get my stm32l486RG to work wtih a microSD car but the SDIO doesnt seem to be alive. I used cubeMX to start up the project but am unable to see any signals on the D0-D4 or CMD lines. Apprec...

STM32F407 Hang in GPIO A 15 Init

Posted on November 30, 2017 at 20:36Hello friends The microcontroller will hang after the following commandHow can I fix this problem? GPIO_InitStruct.Pin = GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL;...

Pedram by Associate III
  • 977 Views
  • 1 replies
  • 0 kudos

STM32F4xx CAN Bus error

Posted on November 30, 2017 at 10:57Hello ,I am working on STM32F4xx CAN interface with Busmaster . Here is my initialization code: /* CAN cell init */CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;/* CAN Baudr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.