STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Overflow interrupt don't trig stm32f1

Hello, I have a problem currently, I am a beginner on stm32 and I would like to create a pulse counter but I cannot get the interrupts from my timer 3 to increment my variable. I don't understand then that the function is indeed carried out but it is...

Resolved! Avalonia UI?

Hi All - Not sure if this is the right place to ask this, but thought I would try anyway.I just finished a project that used Avalonia UI (C# based cross platform system for application GUIs) on a raspberry-pi 4 with a Waveshare touch screen attached....

clawton by Associate
  • 2788 Views
  • 2 replies
  • 2 kudos

Resolved! Why OTG_HS USB/USBX Host on STM32U5Axx just does not work? (2)

I encountered a problem while desperately trying to make USB OTG_HS Host configured on a new Nucleo-U5A5ZJ-Q using CubeMX and ThreadX+USBX. I know that this board is not designed to provide USB power, but this can be overcome with undocumented SB8-10...

USBX-D.png USBX-B.png
TDJ by Lead
  • 17713 Views
  • 32 replies
  • 8 kudos

Resolved! How to use the HAL I3C Library

HelloI'm using NUCLEO-H503 to make an I3C master, and I have some issues.1. I sent the ENTDAA command for I3C communication, but it does not go to HAL_I3C_STATE_READY.The code written after several attempts is as follows.HAL_I3C_Ctrl_DynAddrAssign(&h...

sh.lee by Associate II
  • 6521 Views
  • 6 replies
  • 4 kudos

STM32U599 PA11 as input

Hey, I have a U599 and would like to use the PA11 pin as an input with a pull-up. I've set the CR1_FORCE_USBPWR, USBPWREN, and VDD11USBDIS bits. However, the pull-up voltage only reaches 1.21V in this configuration. The pin works fine as an output.  ...

AGeis.4 by Associate III
  • 4238 Views
  • 8 replies
  • 1 kudos

Alternate microcontroller for STM32G431RBT6

Hello,Would you please suggest us alternate microcontroller for which should be the advance version of STM32G431RBT6 and operating voltage should be more than 105 Celsius.best regards,Nisha Yadav @Peter BENSCH

ny851 by Associate II
  • 4468 Views
  • 9 replies
  • 3 kudos

Resolved! STM32H723ZGT6 ADC stuck after first sample

I'm trying, unsuccessfully, to get a simplest single-channel single-ended polling-the-ADC example going on the nucleo h723 eval board.At first I started bare-metal in assembler from the datasheet, but couldn't get the second ADC sample to fire no mat...

n719z by Associate
  • 3196 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.