STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H563 FDCAN system bootloader

Hi,i'm trying to upload my firmware with FDCAN system bootloader in STM32H563.As this article(https://community.st.com/t5/stm32cubeprogrammer-mcus/fdcan-programming-support/td-p/199854) says that ST link debugger and STM32 cube programmer don't suppo...

Hoon by Associate
  • 1855 Views
  • 1 replies
  • 0 kudos

AN5293 migration F7 - H7: identical peripherals if not mentioned?

Heyho,just checking the migration guide AN5293 for some peripherals I have not yet ported from F7 to H7:if not mentioned in the document, are the peripherals completely and 100% identical (registers & bits) ?Just checked for I2C, and it is not mentio...

LCE by Principal II
  • 2414 Views
  • 4 replies
  • 1 kudos

More than one DSMPS on one MCU

I have developed a custom controller that uses the STM32G474RE to regulate the output voltage of two power supplies.I am now developing the code to implement a peak-current mode controller for each of the two power supplies.  Is there a way that I ca...

Resolved! ADC error

I have connected 100k NTC  with 100K PU resistance. ADC is measuring voltage on NTC is 1580 mV. While multimeter shows 1410 mV. 1410mV is correct number as it gives 32 degC  temperature.I am using ADC in polling mode. I added HAL_ADCEx_Calibration_St...

Nico3 by Senior
  • 7722 Views
  • 6 replies
  • 6 kudos

two independent CAN

HI,I'm working with a micro from the H7 family (H723).I have to implement CAN communication on two distinct peripherals (FDCAN1 and FDCAN2) in interrupt mode but the system doesn't work.Below are the settings I use in my project: void MX_FDCAN2_Init(...

UVagl.1 by Associate II
  • 1680 Views
  • 2 replies
  • 2 kudos

Firmware

Hii everyone!We are working on CAN , and MCU is stm32f103When we are taking output on blue-pill Tx and Rx pin Data is comingBut when are are doing same on custom board data is not showing ,we are uploading same firmware and clock configuration is als...

Resolved! MCU hung after staying idle for hours

In our system with SMT32G041F6P6 powered by a battery, device gets to hung state when kept idle for few hours or days (randomly). We have already implemented a window  watchdog to detect any faults. Even with watchdog enabled, we are getting this han...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.