STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Zephyr B_U585I_IOT02A BLE examples timeout and crash

I'm trying to run a few of Zephyr's BLE examples on the B_U585I_IOT02A development board.   I have tried the beacon, peripheral, and peripheral_csc examples.   These BLE examples all work properly on a Nordic nRF52840 dev board.Zephyr's blinky exampl...

STM32F407VET6 DEMCR base address

Good morning,I'm trying to develop a simple Hello World printf example by writting "Hello World" into the port0 of ITM. There are several tutorials telling that 0xE000EDFCU is the base address to set the bit TRCENA to 1. However, when I try to debug ...

Gonzalo by Associate
  • 2686 Views
  • 3 replies
  • 0 kudos

Resolved! hash registers not defined in stm32h723xx.h

I am trying to use the cryptographic hash processor on the STM32h723xx, however, I cannot find the registers like HASH_CR defined in the device header files.Can someone please advise If I should be using the register definition from another MCU devic...

DEska.1 by Associate II
  • 1278 Views
  • 1 replies
  • 0 kudos

Resolved! USB Device using PA9

I want to use STM32F407V in USB device MSC mode. The device has battery to run the MCU. To fetch data from device, it will be connected to LAPTOP by USB cable.Please confirm below configuration for schematic1) Connect PA9 to VBUS on USB connector,  p...

Nico3 by Senior
  • 2742 Views
  • 2 replies
  • 2 kudos

Resolved! MCUBoot on nucleo H563

Hello,I'm working with the nucleo_h563zi board and Zephyr (3.6).  I'm trying to build using MCU Boot and firmware update. I  have been able to successfully build MCUBoot and flash it to the device. That boots but fails with the "Unable to find bootab...

srberard by Associate
  • 2945 Views
  • 1 replies
  • 0 kudos

SPI periodically receiving wrong data

Hello,I have a custom board with a STM32L010C6 MCU, which periodically reads 3 bytes (24 bit array) from an external component through SPI.I only need SCLK and MISO since the frame resets using a timeout.I configured the SPI as Only-Receiving Master,...

cgallardo_0-1709047504249.png cgallardo_1-1709047623896.png
cgallardo by Associate II
  • 4828 Views
  • 4 replies
  • 1 kudos

STM32L031G6x stop mode power consumption issue

Hello.The MCU currently in use is STM32L031G6X.In order to minimize current during sleep, the external circuit currently uses 100K pull-down to PB3 to set it to "Rising Interrupt" and UART 1 for testing.When measuring the current, remove the external...

Palmer by Associate
  • 1734 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.