2024-02-28 7:12 PM
When I send data from esp32 to stm32, it works fine. But when esp32 initially receives data from stm32 using uart, the data seems to have some random characters.
When i send 75, it looks like this in serial monitor:
Received: %$^#^12
Received: 12
Received: 12
I used KeilC and ArduinoIDE. I just want to get "Received: 12" from stm32. This is my code:
esp32:
#include <HardwareSerial.h>
#define UART_TX_PIN 17 // TX
#define UART_RX_PIN 16 // RX
int d1 = 7;
int d2 = 5;
char tx_array[10];
int flag = 0;
HardwareSerial SerialUART(2); // Create an instance of HardwareSerial for UART1
void setup()
{
Serial.begin(115200); // Initialize Serial Monitor for debugging
SerialUART.begin(115200, SERIAL_8N1, UART_RX_PIN, UART_TX_PIN); // Initialize UART1
}
void loop()
{
tx_array[0] = d1 + '0';
tx_array[1] = d2 + '0';
tx_array[2] = '\n'; // Line feed character
//tx_array[3] = '\0'; // Null terminator
SerialUART.print(tx_array);
if (SerialUART.available()) {
String receivedData = SerialUART.readStringUntil('\n'); // Read until newline
if (receivedData != "") {
// Process received data
Serial.println("Received: " + receivedData);
}
}
delay(500); // Add a small delay to prevent flooding the buffer
} and stm32f103c8t6:
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdio.h"
#include "string.h"
#include "stdlib.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
char tx_buffer[10] = {0};
char rx_buffer[10] = {0};
char rx_array[10] = {0};
char result[10] = {0};
int received_value1;
int received_value2;
uint8_t count = 0;
uint8_t data = 0;
volatile uint32_t delayCounter = 0;
#define DELAY_THRESHOLD 500
UART_HandleTypeDef huart1;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
char* fuzzy_logic_func(char input_array[])
{
input_array[strlen(input_array)] = '\0';
received_value1 = input_array[0] - '0'; //char to int
received_value2 = input_array[1] - '0';
int result_var = received_value1 + received_value2;
sprintf(result, "%d", result_var);
strcat(result, "\n");
delayCounter++;
HAL_UART_Transmit(&huart1, (uint8_t*)result, strlen(result), 100);
return result;
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
rx_buffer[count] = data;
count++;
if (data == 10)
{
for(int i = 0; i<10; i++)
{
rx_array[i] = rx_buffer[i];
rx_buffer[i] = 0;
//count = 0;
}
count = 0;
fuzzy_logic_func(rx_array);
}
HAL_UART_Receive_IT(&huart1, &data, 1);
}
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
HAL_UART_Receive_IT(&huart1, &data, 1);
while (1)
{
if (delayCounter >= DELAY_THRESHOLD)
{
// Perform actions that were delayed
// Reset the delay counter
delayCounter = 0;
}
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief USART1 Initialization Function
* @param None
* @retval None
*/
static void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
/* USER CODE BEGIN USART1_Init 1 */
/* USER CODE END USART1_Init 1 */
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART1_Init 2 */
/* USER CODE END USART1_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2024-02-29 4:12 AM - edited 2024-02-29 4:13 AM
Check by oscilloscope or logic analyzer Tx signal from STM32. When you use internal oscillator, signal timing can be out of tolerace.Or some garbage is in the transmit buffer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.