STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LPDMA Update Link Error

  static uint16_t aDST_Buffer_1[BUFFER_SIZE] = {0}; static uint16_t aDST_Buffer_2[BUFFER_SIZE] = {0}; LL_DMA_LinkNodeTypeDef pNode1, pNode2; /** * @brief LPDMA1 transfer configuration * @PAram None * @retval None */ void BspLPDMA1Init(void) { /*...

Resolved! What is USART CTS latency?

I am starting a product design tentatively using the STM32F072RBT6.I want to determine how soon the CTS input must go low to prevent the USART from transmitting the next byte.Even informed opinion would be appreciated; but a reference to documentatio...

usart clocks.jpg

Resolved! STM32L433 VREFINT_CAL Value

Hello,I'm trying to work with the ADC of the STM32L433 microcontroller. The Reference manual (RM0394) on page 448 it says : The following formula gives the actual VDDA voltage supplying the device:VDDA = 3.0 V x VREFINT_CAL / VREFINT_DATAWhere can I ...

RStra by Associate III
  • 3089 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G473VC

Hello,I will use stm32g473VC ADC2 working together with DMA.I configure ADC2, Input3 at Pin PA6 and DMA2 Channel1 to read 100 Samples from ADC after Start.At first call after cpu reset I receive the expected result:ADC:Value 4034 for Items 0->99, as ...

jhoerd by Associate II
  • 1476 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 VCAP pin problem

 Hello,I have designed a PCB with 3 STM32H725VGT6 MCUs, and assembled them according to my schematic:(sorry for this resolution, this is from a converted pdf)All 3 MCUs are the same, from this schematic.R5 and R2 are just 0R jumpers to select the boo...

schmtc.png
fing by Associate III
  • 6971 Views
  • 5 replies
  • 3 kudos

Resolved! STM32H7 RM0399 Rev4 FDCAN Typos?

Looks to me like the FDCAN peripheral has a few registers that are marked 'r' when they are likely 'rw' in the RM. They are the registers that configure the size of the FDCAN messages. This isn't blocking my work; only thought the ST team should know...

Screenshot 2024-02-29 at 09.13.44.png Screenshot 2024-02-29 at 09.13.55.png

Remote wakeup on STM32F0

Trying to implement a composite HID device on STM32F042 (or maybe STM32F072 as both Flash and RAM usage seem insane), starting from the MX mouse middleware. After much scratching around it's finally working as a mouse and keyboard and I now need to a...

DMA and Direct Mode

Posted on August 07, 2013 at 21:21 I'm confused about the FIFO error flag (FEIF) when I set up DMA for direct mode transfers. As I understand it, in direct mode the FIFO is disabled. But for some reason, if I enable the FE interrupt in the DMA_S...

andprice by Associate II
  • 5239 Views
  • 7 replies
  • 1 kudos

Resolved! STM32L412K8 Exposed Pad question

Hi!I'm an EE designing a PCB. Referencing the datasheet: https://www.st.com/resource/en/datasheet/stm32l412k8.pdfSection 7.4 on page 178, UFQFPN48, the Exposed Pad (EP) says that it should be connected to GND.Section 7.6 on page 184, UFQFPN32 (the ch...

EngPete by Associate
  • 2781 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.