STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unable to Connect to a Custom H725RGV6 Board

Hi all, recently I made a board with H725RGV6, but when I tried to flash a test firmware for the first time, I got " Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication" fro...

sche.png
Leonana69 by Associate II
  • 2766 Views
  • 3 replies
  • 0 kudos

Resolved! Azure RTOS Integration in B-U585-IOT2A Bootloader Environment

Hello ST, I am trying to integrate ThreadX into TFM_Appli-NonSecure project. Mostly I am able to integrate it and execute but to make a thread run, I have to comment _tx_initialize_low_level(); API in _tx_initialize_kernel_enter() function.This all w...

Nitin by Associate III
  • 9236 Views
  • 17 replies
  • 6 kudos

Issue with STM32G0: Intermittent ADC Data Reading. Spikes to 0

Hello everyone,I’m working with an STM32 G0 microcontroller and encountering an issue with reading data from two sensors. One of the sensors provides consistent and accurate readings, however, the second sensor shows intermittent spikes to zero in th...

4be05f0a-356c-4b77-8063-3e2fe09b96fc.jpeg
esxu by Associate III
  • 3467 Views
  • 3 replies
  • 0 kudos

Resolved! Fastest ADC measures with DMA

I'm using a Nucleo-G474RE to measure a signal via ADC1.ADC measures are triggered by TIM2, then transferred via DMA1 into a large buffer (60KB).When the buffer is full an interrupt is generated and I give the DMA another 60KB buffer.After that, every...

0xfab by Associate II
  • 3448 Views
  • 2 replies
  • 1 kudos

Resolved! USB CDC data loss

Hello,I am trying to transmit some data on my STM32F042F6P6. But my PC's serial monitor only picks up some of it. Here is the code and the serial monitor output:void readAllRegs(void){ uint8_t value; for (uint8_t addr = 0x00; addr <= 0x2E; addr++...

LLope.31 by Associate III
  • 6787 Views
  • 7 replies
  • 1 kudos

How to Check HSE is Connected To STM32

Hi,I am using STM32F205 Board for our development. We were using HSI (16MHZ) as the clock and found out that HSI has issues with high temperatures. I am calibrating HSITRIM value to fix the clock drift issue and we already have 50 boards manufactured...

JThom.15 by Associate III
  • 6653 Views
  • 8 replies
  • 4 kudos

Resolved! Write data in custom flash section

Hi,I'm working on stm32l496 and I try to write data to a custom flash section, in the .ld file I put new sector :/* Memories definition */MEMORY{[...]FLASH (rx) : ORIGIN = 0x08003800, LENGTH = 0x07B800config(rx) : ORIGIN = 0x0807F000, LENGTH = 2Kcomm...

K-C by Associate II
  • 7702 Views
  • 6 replies
  • 0 kudos

Resolved! STM32U5 SAI in I2S mode + GPDMA

Hi,I have a board with an STM32U575 at the core.I'm attempting to set up SAI receiver in I2S mode, with 32-bit 48kHz sampling. See my configuration of SAI A below: I also want to receive the data continuously in circular mode via DMA (or GPDMA in th...

Screenshot 2024-02-06 at 05.31.13.png Screenshot 2024-02-06 at 05.33.01.png Screenshot 2024-02-06 at 05.56.49.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.