STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PUPDR in GPIOD - default values are wrong

In the manual it states, that reset value is 0x000.., and that 0xFFFF... is reserved. But when debugging, i see, that it is 0xFF... . When now assigning a new value to it via HAL_GPIO_Init(), the register does not take the new values.Hold on!I just f...

Tobe by Senior III
  • 1371 Views
  • 1 replies
  • 1 kudos

ADC multichannel DMA with Freertos on STM32H735G-DK

I have tried many things but cannot seem to get ADC multichannel DMA with Freertos on STM32H735G-DK working.I have setup the ADC to use DMA following many tutorials. I have set up a task to start the ADC with DMA, but the conversion complete callback...

CYBR by Associate II
  • 1415 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H5 I3C ENTDAA waveform

Hello! I have a H563ZI and a KEYSIGHT oscilloscope.I configured H563ZI as controller and sent an ENTDAA , then problem occired:        1.slave updated its dynamic address which as same as static address and different with what i set.         2.there ...

Xonier by Associate III
  • 2558 Views
  • 4 replies
  • 2 kudos

interrupt are miss or not ?

Hello STM32 community,I am currently working on a project utilizing the STM32H757 microcontroller, which boasts 8 UART interfaces. In my application, I have configured all UARTs to operate in interrupt mode for receiving data.My concern arises when m...

Resolved! Running a function on ram

#define EEPROM_SEC __attribute__((long_call, section("EepromSection")))EEPROM_SECint add(int a, int b) {return a + b;}static __attribute__(( aligned(32))) uint32_t code_buf[20] = { 0 };//...int main(void) {HAL_Init();SystemClock_Config();MX_GPIO_Init...

Resolved! STMG01 Baremetal UART not Working

Hi, I wonder has anyone experience with baremetal USART implementation as I have attached a Source file for USART for a 'STM32G0B1RET' discovery board but it just sits there and doesn't transmit anything? See attached (usart.c). I have basically just...

PLee.3 by Associate III
  • 4209 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.