STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VBUS Detection on STM32F769i Discovery Board

Hi team,              I am using stm32f769 discovery board for implementing OTG HS(MSC) on it. After seeing it's schematic am bit confused regarding the VBUS pin handling. According to the below schematic VBUS is handling by USB3300 PHY.I. VBUS Handl...

Shikamaru_0-1709191923215.png Shikamaru_1-1709192049328.png Shikamaru_3-1709192480846.png
Shikamaru by Associate III
  • 1791 Views
  • 1 replies
  • 0 kudos

Resolved! Strange behavior - HW probelms?

  Hello to everyone. I'm working on a display interface, changing from M3 -> M4 -> H5 CPUs. The issue appeared on all type(it's a HW issue?) At the beginning I can connect, debug, program and so on. Bt after some operation, I can't continue. I stil...

STTwo32_0-1712143149106.png STTwo32_1-1712143149076.png
TheRaprus by Associate III
  • 2633 Views
  • 4 replies
  • 4 kudos

Resolved! Proper way to use a Library (.a)

Hi everyone,Designing the BLE (bluetooth low energy) part of my software, I have to use BlueNRG-1, BlueNRG-2 DK SW package.First of all, I included by hands the library file (.a).But there is a lot of source-code that is not provided in the library (...

Resolved! stm32H503RB Determination of I3C IBI payload size

Hi,I am using the nucleo-H503RB I3C (Controller mode) with this example to connect to an I3C standard chip. The sensor transmits IBI with 5 bits of payload but I noticed that the STM32 receives only 4 bits, and then it stops receiving the fifth bit.I...

Hexu by Associate II
  • 2876 Views
  • 3 replies
  • 2 kudos

Programming original stm32f103c8t6 with clone bluepill board

Hi everyone i bought bluepill with fake chip and i replaced it with an original stm32f103c8t6.When i use stlink utility with other fake bluepill it detecets the chip but when i use stlink utility with original chip in a fake bluepill board i get this...

Ahmetp_0-1712139532794.png
Ahmetp by Associate II
  • 5518 Views
  • 5 replies
  • 0 kudos

Resolved! JTAG

Hi,We are currently working with the STM32G0B1VET6 Microcontroller and have been designing connections for the SWD interface. However, upon verifying the datasheets, we couldn't find any mention of a JTAG interface for debugging purposes.Could you pl...

Fake STM32 chip?

Hi, I have a help  we purchased with your chip, but it seems that it is fake, please let me know if the name or engraving is printed on your chip? Thank for your support 

DianaSok by Associate II
  • 3104 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.