2023-05-29 1:45 AM
Hello everybody! I have a sine-wave array, that I throw to the DAC, triggering it by TIM6. When the TIM6 interrupt routine is responsible for supplying samples - everything works fine, but when I try to use DMA nothing works. The DMA keeps spitting the USEF error. Please help! I have been trying to figure out what to do for several days already. For testing purposes, I just try to make a one 16-bit variable transfer via DMA to no avail. If anybody would please give me some advice.
void DAC_init(void){
RCC->AHB3ENR |= RCC_AHB3ENR_DAC1EN; //Connecting DAC to the bus
DAC1->CR &= ~(DAC_CR_EN1); //Disable the DAC before applying settings
DAC1->MCR |= DAC_MCR_HFSEL_0; //Must set this bit, since AHB frequency is >80Mhz
DAC1->MCR |= DAC_MCR_SINFORMAT1 + DAC_MCR_SINFORMAT2; //DAC now accepts signed numbers (no need to apply bias)
TIMER_dac_init(); //Setting up the timer for triggering DAC
DAC1->DHR12LD = 128; //Before the DMA request is generated it is necessary to perform the first write.
DAC1->CR |= DAC_CR_TEN1 +(5 << DAC_CR_TSEL1_Pos); //DAC channel1 will be hardware triggered by the timer 6
DAC1->CR |= DAC_CR_DMAEN1; //Enable DMA for the channel 1
DAC1->CR |= DAC_CR_EN1; //Enabling DAC channel1
static short i = 32000;
GPDMA1_Channel14->CCR &= ~(DMA_CCR_EN); //Disable DMA channel
GPDMA1_Channel14->CCR |= (DMA_CCR_PRIO_1); //Set DMA channel priority
GPDMA1_Channel14->CTR1 |= (DMA_CTR1_DDW_LOG2_0 + DMA_CTR1_SDW_LOG2_0); //The data is 16-bit wide (DAC accepts 16-bit numbers in SIGNED mode and ignores the 4 bits
GPDMA1_Channel14->CTR2 |= (DMA_CTR2_DREQ + (2 << DMA_CTR2_REQSEL_Pos) + DMA_CTR2_BREQ); //Channel request is driven by destination, DMA trigger, Block transfer mode
GPDMA1_Channel14->CDAR = (volatile long unsigned int)(&(DAC1->DHR12LD)); //Set DAC as the destination for GPDMA transfer
GPDMA1_Channel14->CSAR = (volatile long unsigned int)&i; //Pointing DMA at the source data location
GPDMA1_Channel14->CBR1 |= (1 << DMA_CBR1_BRC_Pos); //Block is transferred just once
GPDMA1_Channel14->CBR1 |= (1 << DMA_CBR1_BNDT_Pos); //Transfer 2 bytes per block (16-bit data)
GPDMA1_Channel14->CCR |= (DMA_CCR_EN); //Enable DMA
}
Solved! Go to Solution.
2023-05-30 1:15 AM
I've cracked it!
This value: "DMA_CTR1_DDW_LOG2_0" should be changed to this: "DMA_CTR1_DDW_LOG2_1"
Apparently DAC only accepts the world-aligned access.
And also one more mistake here: "1 << DMA_CBR1_BNDT_Pos" should be: "2 << DMA_CBR1_BNDT_Pos" because we transfer 2 bytes at a time, not one byte. F@^%k my old boots, haha!! Spent nearly two days figuring this out! Hopefully someone will find this story revealing.
But I still don't understand and would be grateful for any comments. The Guide says: "As DAC_DHRx to DAC_DORx data transfer occurred before the DMA request, the very first
data has to be written to the DAC_DHRx before the first trigger event occurs."
Does it mean that during DAC init I must write some dummy value to DAC_DHRx in order to make the DMA thing running? I just cannot understand... Everything seems to work without it though.
2023-05-30 1:15 AM
I've cracked it!
This value: "DMA_CTR1_DDW_LOG2_0" should be changed to this: "DMA_CTR1_DDW_LOG2_1"
Apparently DAC only accepts the world-aligned access.
And also one more mistake here: "1 << DMA_CBR1_BNDT_Pos" should be: "2 << DMA_CBR1_BNDT_Pos" because we transfer 2 bytes at a time, not one byte. F@^%k my old boots, haha!! Spent nearly two days figuring this out! Hopefully someone will find this story revealing.
But I still don't understand and would be grateful for any comments. The Guide says: "As DAC_DHRx to DAC_DORx data transfer occurred before the DMA request, the very first
data has to be written to the DAC_DHRx before the first trigger event occurs."
Does it mean that during DAC init I must write some dummy value to DAC_DHRx in order to make the DMA thing running? I just cannot understand... Everything seems to work without it though.
2024-04-11 4:43 AM
I had the same problem and change the DMA size to word and it works.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.