STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CubeMX STM32L4 code generation question

Hi folks,I use MX to generate a code for STM32L4. I noticed, when I configure timer in one pulse mode, I cannot set OC CH1 in PWM mode with CubeMX. I could set it manually after code was generated, but it would be overwritten if I run MX one more tim...

Lex by Associate III
  • 1250 Views
  • 1 replies
  • 1 kudos

SPI - not recieving a response on MISO line

Hello everyone!I'm trying to communicate with a slave device (ICM-42688-P: https://invensense.tdk.com/wp-content/uploads/2020/04/ds-000347_icm-42688-p-datasheet.pdf), but I don't recieve anything on the MISO line. I'm using the nucleo-wb55rg for the ...

AndrasToth_2-1713191910613.png AndrasToth_3-1713191981610.png

customized keyboard using stm32 f44 series controller

Hello everyone,as I am developing keyboard with extra keys adding to the existing key board. I am adding extra modifier keys to the key board to perform the task. kindly let me know will it work and give suggestion inputs. my customized keyboard cons...

SSRIN.2 by Associate III
  • 4172 Views
  • 7 replies
  • 4 kudos

Resolved! How to get the value of the program counter ?

Hello, Sometimes I have my stm32F7 going in hardfault_handler, so for my customers I have to display on a screen the last address where the software crashed, then I can analyse which problem occure the crash. So I want to get the value "pc" (program ...

PierreG-S by Associate II
  • 4169 Views
  • 2 replies
  • 2 kudos

Resolved! STM32u585 Memory Mapped Read/write on B-U585I-IOT02A

While using memory mapped mode for APS6408L using STM32u585 on B-U585I-IOT02A, how is the row boundary crossing handled?* If I want to write across multiple Rows in memory mapped mode, do I need to handle this manually or is it automatically handled ...

Bootloader v11 + changes

I've been using an STM32G474xx in a project for a few years now and have a function that jumps to the bootloader. It seems in a recent rev of the chip the bootloader has changed. I'm finding that I can no longer jump to the bootloader similar to how ...

PCarn.1 by Associate III
  • 1724 Views
  • 2 replies
  • 0 kudos

Failure when migrating STM32CubeMX project to compatible part

I have tried to migrate an STM32CubeMX project from the STM32H747AIIx to the STM32H747XIHx using the procedure described here:How to switch from one STM32 to another using STM3... - STMicroelectronics CommunityIt failed with the following error messa...

ACaru.1 by Associate II
  • 1691 Views
  • 2 replies
  • 0 kudos

Resolved! Debouncing

Can anyone help me with debounce code in C for Rising and falling edge interrupt??

sne_123 by Associate III
  • 26361 Views
  • 20 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.