2024-04-17 2:43 PM
I have tried to migrate an STM32CubeMX project from the STM32H747AIIx to the STM32H747XIHx using the procedure described here:
How to switch from one STM32 to another using STM3... - STMicroelectronics Community
It failed with the following error message:
"Project Import failed: Import 'STM32H747AIIx' not supported (multiple context)"
Any idea what is wrong???
I am using STM32CubeMX v6.11.0 with firmware package STM32Cube FW_H7 V1.11.1, on Windows 11.
2024-04-17 3:05 PM
Do you have a more concrete part number? For example use STM32H747AII6 instead of STM32H747AIIx and STM32H747XIH6 instead of STM32H747XIHx?
2024-04-17 3:09 PM
Yes, in fact the part numbers are STM32H747AII6 and STM32H747XIH6 (CubeMX, however, shows them as STM32H747AIIx and STM32H747XIHx).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.