STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

connecting STM32U5A9NJH6Q DSI pins to unpowered LCD

I have designed an STM32U5A9NJH6Q into a custom board for a medical device.  The display is working great in the first rev of the boards.  In the next revision of the boards, I have been asked to add the capability to power off the LCD display.  Are ...

Resolved! Will DVP camera interface support STM32H747 MCU

most of the cameras in th market are with DVP and MIPI CSI interface, do DVP camera interface supports STM32H747 microcontroller, if so to which pins can we connect DVP to DCMI interface.

kumar30 by Associate II
  • 3490 Views
  • 2 replies
  • 0 kudos

STM32H563, PDM and DMA Double buffering

Hello,i would like to read output from a digital microphone using SAI, DMA and double buffering technic. transfert are done and callbacks are triggering properly.  The problem is got is either Half cplt or Full cmplt callback interrupt being called t...

jboui.1 by Associate II
  • 5880 Views
  • 11 replies
  • 0 kudos

Resolved! the pin to pin compatible part of stm32f103vet6?

Hi,I'm using stm32f103vet6 in my design, but due to the limit power budget, the MCU consumes much power(60mA per MCU , while I used 2 chips in my design), result in frequently triggering over current protection. Is there pin to pin compatible STM32L ...

JKW by Associate III
  • 6830 Views
  • 10 replies
  • 9 kudos

Resolved! Most Efficient solution for reading ADC through SPI

Hi,i'm always looking for the most efficient implementation of code in my STM controllers and was wondering which is the most efficient way to implement ADC reading from an external ADC chip trough SPI in an STM32G4 controller.The ADC (MCP3461/2/4) h...

sde c.1 by Senior II
  • 6934 Views
  • 6 replies
  • 1 kudos

Resolved! USB Host "ALL Classes"

Hello everyone, I'm a bit confused about using USB.I need to use the USB port both to create a CDC connection with a PC and to read/write data from USB flash drives.Initially, I wanted to create a project that could handle both HOST and DEVICE modes,...

SDall.11 by Associate III
  • 3312 Views
  • 4 replies
  • 1 kudos

Resolved! No DMA Callback in I2S DMA Half Duplex Transit

I am using a Nucleo F401RE board to drive a PCM5102a PCM Audio Codec via I2S.My goal is to send data from a double buffer via DMA.Since I am only using the Audio Codec as an output, I configured my I2S as Half-Duplex Master in CubeMX.Now to my proble...

95lux by Associate II
  • 2251 Views
  • 2 replies
  • 1 kudos

I2C or I3C for broadcast communication - STM32H503RBT6

Hello!In my project, I have one "Mother board" and other four "Child boards".Both boards are using STM32H503RBT6 microcontrollers.There needs to be a communication between the Mother (master/controller) and the Child (slave/target). Child to Child wo...

mpires_0-1714659763974.png
mpires by Associate II
  • 4056 Views
  • 6 replies
  • 3 kudos

Resolved! STLink emulator with Stop mode condition

Hi everyone,I have a problem, let's see if someone can help me...I have a board that works with an STM32L053xxxx, my application, at a certain point, enters stop mode. Here comes the problem, the emulator disconnects.Is there any technique or emulato...

davide_mp by Associate II
  • 3203 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.