STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H725 ADC

Hello team, I am using the default generated code on STM32H725 uC for ADC1. I am using it in polling mode. The value what I get in ADC DR is 10 times less than the value that I expected. I tried this for various voltage range on its external pins. I ...

Resolved! STM32F405RGT6 CAN Reception Problem

I have been trying to resolve the issue for receiving the CAN interrupt but not able to find the root cause.Hardware is a custom board micro is STM32F405RGT6 i am using CAN1 for CAN communication with 500 Kbps.Able to transmit message CAN message usi...

STUser34_0-1715707247933.png STUser34_1-1715707347339.png STUser34_3-1715707652000.png STUser34_4-1715707732840.png
STUser34 by Associate III
  • 4699 Views
  • 9 replies
  • 3 kudos

Resolved! Portenta H7: external debugger

Some people might ask: "how to connect a debugger on Portenta H7?"the Portenta H7 MCU module does not have a debugger connector (just tiny solder pads)you need the Breakout Board, or the Vision Shield (both provide the debugger header)STLINK-V3 comes...

Portenta_H7_debugger.png
tjaekel by Lead
  • 1784 Views
  • 1 replies
  • 1 kudos

Need reliability data for the part STM32L071KZU3

Hi,   I require assistance in finding the reliability data for the products. I have search through the website but regrettably, I have not been able to find the required information. The components of interest are identified by the part number STM32L...

STM32g0b1keu6 controller FCAN issue

Hello i am trying to configure STM32g0b1keu6 for extended ID but i am not able to get any messages on my PCAN view window. Also i observed the TXBAR bit is not setting at all, as it represents the transmit request field. Can anyone help me with the s...

How to update STM32F401 firmware over LTE/GSM ?

Greetings.For our data collection devices, we use STM32F401 as the microprocessor and Telit modems to communicate with the server. We are planning to have a feature to update the firmware on the STM32F401 over the air, if possible. Currently we use S...

RNair.3 by Associate
  • 7504 Views
  • 10 replies
  • 3 kudos

MCU temperature

I'm working on a project with the STM32G4 MCU. I want to know the maximum temperature at which the MCU can operate at full power. What is the corresponding internal MCU temperature for that value? What does the temperature information in the above i...

Locnvselex_vn_0-1715518273613.png

STM32F746 USB Device MSC DMA Problem

Hi, I am using STM32F746G_DISCO, STM32 CubeMX version: 6.11.1, STM32CubeIDE version: 1.15.0 and FW_F7 firmware package V1.17.1.I tested the project: \STM32F746GDISCOVERY\STM32Cube_FW_F7_V1.17.0\Projects\STM32746G-Discovery\Applications\USB_Device\MSC...

1.png
Alex_777 by Associate III
  • 3656 Views
  • 7 replies
  • 3 kudos

Resolved! Long Period Timer PWM Setup

Hello,I am attempting to set up a timer PWM output to have a set 600s period with a variable duty cycle based on a potentiometer input using an STM32G030J6 MCU.  I've setup PWM output timers before will little difficulty but this time I'm having a di...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.